|
Description The documentation included in this entry describes how to connect a SIMATIC MV440 code reader device to a SIMATIC S7-300 using PROFINET IO.
In this example, a CPU315-2PN/DP is used as PROFINET IO controller.
The figure below illustrates this device configuration.

Fig. 01
Documentation
DP_PROFINET_IO_with_MV440_or_MV420_en.pdf ( 3400 KB )
Sample programs The downloadable "MV4x0_PROFINET_sample_project_V1_0.zip" file provides you with the following sample program including all the necessary components:
- The "MV4x0_PROFINET_sample_project_V1.0.ap11" project that was created with STEP 7 (TIA Portal)V11 and includes the configuration of a CPU315-2PN/DP as PROFINET IO controller and a SIMATIC MV440 code reader device as PROFINET IO device.
- Block "FB79_Application[FC1]", which is called in the user program of the CPU.
MV4x0_PROFINET_sample_project_V1_0.zip ( 2031 KB )
Configuration files The downloadable "ConfigurationFiles.zip" file provides you with the configuration files for the code reader devices below:
| Code reader device |
Configuration file |
| MV440 SR |
MV440SR_PROFINET.xml |
| MV440 HR |
MV440HR_PROFINET.xml |
| MV440 UR |
MV440UR_PROFINET.xml |
| MV420 SR-B |
MV420SRB_PROFINET.xml |
| MV420 SR-P |
MV420SRP_PROFINET.xml |
ConfigurationFiles.zip ( 1948 KB )
Creation environment The screens and downloads in this FAQ were created with STEP 7 (TIA Portal)V11.
Note on security
Caution The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. Further information can be found in Entry ID: 50203404. |