show the entry list

STEP 7 (TIA Portal) -- Setting up development environments -- Installing / transferring licenses 
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12? 
Why is the license not recognized when opening STEP 7? 

Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?Go to beginning
Part number:

Description
If you still do not have a version of STEP 7 installed on your computer, you need the full license for STEP 7 Basic V12 or for STEP 7 Professional V12. If you have a version of STEP 7 installed on your PC, you need either the license for the upgrade or for the PowerPack. The table below shows the different licenses needed for a new installation or for updating your version of STEP 7.
 
Case Procedure
1 No version of STEP 7 installed on your computer.
  • For STEP 7 Basic V12 you need the floating license with order number: 6ES7822-0AA02-0YA5
  • and for STEP 7 Professional V12 you need the floating license with order number: 6ES7822-1AA02-0YA5.

You can also install the trial license for each product:

  • Order number 6ES7822-0AA02-0YA7 for STEP 7 Basic V12.
  • Order number 6ES7822-1AA02-0YA7 for STEP 7 Professional V12.

Note
As registered customer you can download the trial for SIMATIC STEP 7 Professional V12 and test it for 21 days. The Professional edition also includes the functions from SIMATIC STEP 7 Basic V12. More information is available in Entry ID: 67639464.

2 You have STEP 7 Professional 2006 or 2010 installed on your computer and you want to upgrade to STEP 7 Professional V12.
  • Here you need the upgrade with the COMBO floating license (order number: 6ES7822-1AA02-0XE5).
3 You have STEP 7 Basic V10.5 installed on your computer and you want to upgrade to STEP 7 Basic V11.
  • Here you need the upgrade with the single license (order number: 6ES7822-0AA01-0YE0).
4 You have STEP 7 Basic V11 installed on your computer and you want to upgrade to STEP 7 Basic V12.
  • Here you need the floating upgrade package license (order number: 6ES7822-0AA02-0YE5).

Note
Valid for STEP 7 V11 Single and for STEP 7 V11 Floating.

5 You have STEP 7 Professional V11 installed on your computer and you want to upgrade to STEP 7 Professional V12.
  • Here you need the upgrade with the floating license (order number: 6ES7822-1AA02-0YE5).

Note
It is not possible to use this upgrade to upgrade from STEP 7 Professional 2010.

6 You have STEP 7 V5.4 or V5.5 installed on your computer and you want to upgrade to STEP 7 Professional V12.
  • Here you need the PowerPack & Upgrade with the floating license (order number: 6ES7822-1AA02-0XC5).
7 You have STEP 7 Basic V12 installed on your computer and you want to change to STEP 7 Professional V12.
  • Here you need the PowerPack with the floating license (order number: 6ES7822-1AA02-0YC5).
8 You have the STEP 7 Professional 2006/2010 Upgrade installed on your computer and you want to upgrade to STEP 7 Professional 2010/V11.
  • Here you need the Combo Floating License (order number: 6ES7822-1AA11-0XE5) for the SIMATIC STEP 7 PROF. 2010/V11 UPGRADE

Note
The requirement here is that an SUS (Software Update Service) is available.

9 You have STEP 7 Professional 2010/V11 installed on your computer and you want to upgrade to STEP 7 Professional 2010/V12.
  • Here you need the Combo Floating License (order number: 6ES7822-1AA02-0YE5) for SIMATIC STEP 7 PROFESSIONAL V12 ENGINEERING SOFTWARE.
Table 01

The floating licenses are also available here for downloading. Entry 67851956 contains the list with the order numbers at the link "STEP_7_V12_Orderlist". The order numbers are linked with the associated downloads.

The table below shows the features of the different license keys that you can order and install.
 
License Key Meaning
Single License Unlimited use on any one computer.
Floating License Unlimited use on any one computer or through the network.
Rental License Limited use as stipulated in the rental contract.
Trial License Limited use (max. 21 days) for tests and for validating (with disclaimer).
Upgrade License An Upgrade License converts a license for an earlier version x to a license for version >x+... .
Table 02

You can also install STEP 7 V5.4/V5.5, STEP 7 Basic V10.5, WinCC flexible 2008 onwards and WinCC V7.0 SP2 onwards in parallel to STEP 7 V12.

  • With an Upgrade License / Combo License for STEP 7 V12 (TIA Portal) you can operate both STEP 7 V5.4/V5.5 or STEP 7 Professional 2006/2010 and STEP 7 Professional V12.
  • With an Full License for STEP 7 V12 (TIA Portal) you cannot operate STEP 7 V5.4/V5.5 or STEP 7 Professional 2006/2010.

Follow the instructions in the table below to upgrade a License Key.
 
No. Procedure
1 Open the Automation License Manager and select "View > Administration".
2 Transfer the Upgrade License Key to the hard disk on which you want to carry out the upgrade.
3 Also transfer the License Key of the previous version to the hard disk if the license is not yet located on your computer.
4 Select the storage location in the navigation area where the license key to be upgraded is located (previous version).
5 In the Object area you select the license key that is to be upgraded.
6 Execute the menu command "License Key > Upgrade...". The upgrade is now made.


Fig. 01

Table 03

Note
More information about licenses and the differences between the authorizations and licenses is available in Entry ID: 19020864

Creation environment
The screen in this FAQ was created with ALM V5.1+Upd 1.

Why is the license not recognized when opening STEP 7?Go to beginning
Part number:

Description
Check whether you have the correct license for your version of STEP 7 installed on your PC. A license is always valid for just one version3). If, for example, you have procured a Field PG with integrated license for STEP 7 Basic V10.5, then you can only open and work with that product. After installing STEP 7 V5.4, you also need a license for STEP 7 version V5.4 if you want to open the SIMATIC Manager3).

If, before the SIMATIC Manager opens, you get the message indicating that no valid license key can be found,

  • then either you have not installed a license
  • or you have installed a license that is not valid for your version of STEP 7. For example, if you have installed the license for V5.4 for STEP 7 V5.5.

Without a valid license you can only open STEP 7 if you activate the Trial License (limited to 14 days). Once the 14 days are over, you can open the SIMATIC Manager again only if you have transferred the license required for your version of STEP 7 to your PC. The table below gives an overview of the software versions. You need STEP 7 or STEP 7 Professional for programming the S7-300/400 modules. For example, you install the license for version V5.4 via the ALM (Automation License Manager).
 
Software versions Product groups Project management Handling via ALM
STEP 7 V5.3 / V5.4 / V.5.5 S7-300 / S7-400 SIMATIC Manager License on USB stick / or floppy disk1)
STEP 7 Professional Edition 2006/2010 (S7-GRAPH, S7-SCL, S7-PLCSIM included) S7-300 / S7-400 SIMATIC Manager License on USB stick / or floppy disk1)
STEP 7 Basic V10.5 S7-1200 TIA Portal License not relocatable, but installed automatically2)
WinCC flexible 2008 Advanced HMI Panels SIMATIC Manager License on USB stick / or floppy disk1)
WinCC Basic V10.5 KTPxxx Basic TIA Portal License not relocatable, but installed automatically2)
STEP 7 (TIA Portal) Basic V11 S7-1200 TIA Portal License not relocatable, but installed automatically2)
STEP 7 (TIA Portal) Professional V11 S7-1200 / S7-300 / S7-400 / WinAC TIA Portal License on USB stick1)
Table 01

1) You can install the licenses when installing the software or later and also uninstall them again. You can store licenses on the following media:

  • License key floppy disks or sticks
  • Local hard disk
  • Hard disks of computers in the network

2) The licenses for these products are supplied on the installation data medium and are installed automatically during installation by the Setup. There is no separate installation storage medium (stick, floppy disk) with licenses and you cannot transfer the licenses to other computers.

3) As from STEP 7 V5.3 the licenses for STEP 7 V5.x are automatically also valid for the earlier versions of the same software.

If you uninstall the STEP 7 V10.5/V11 and WinCC Basic V10.5 products, the associated licenses are also uninstalled automatically with them. You should save any licenses you still need.

You can check whether the license required for your software is installed in the ALM (Fig. 01).


Fig. 01

Note
The ALM is supplied together with the project on the installation medium and is installed automatically during installation of the product. However, you uninstall the software product, the ALM is not uninstalled automatically with it, because the ALM is used for managing the license keys of multiple Siemens products.

More information on licenses for SIMATIC products is available in the following Entry IDs: 19020864, 18561363, 15293567, 19100818 and 21362881.

Creation environment
The picture in this FAQ was created with ALM (Automation License Manager) version V4.0+SP3.

Keywords
Authorization, TIA (Total Integrated Automation)

 Entry ID:56076387   Date:2013-05-06 
I regard this article....as helpfulas not helpful                                 






























related links
What should you take into conside ...
SIMATIC STEP 7 V10.5 SP2
Automation Licence Manager
What should you watch out with re ...
Why does a message appear in STEP ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour