show the entry list
WinCC (TIA Portal) -- Creating HMI configurations -- Working with tags
How can you access tags of an operator panel using an Excel application with WinCC (TIA Portal)?
How can you set up a connection between a LOGO! 0BA7 and an HMI Panel?
How do you specify the runtime of a timer by means of an operator panel and how do you output the remaining runtime?
How do you create dynamic text lists in WinCC (TIA Portal)?
How do you migrate tags from STEP 7 V11 to WinCC V11?
How can you provide new tags for the separate trends of an f(t) trend display by means of a C or VB script in WinCC Runtime Professional V11 and higher?
How do you migrate tags from STEP 7 V11 to WinCC V11?
Part number:

Description
WinCC V11 provides the option of using drag-and-drop or copy-and-paste to migrate PLC tags and elements from a data block from one device to another.

Below we describe how to...

This function saves you a great deal of time when creating an HMI configuration.

Function description
Migrate PLC tags to an HMI tag table.
 
No. Function description
1 Migrate PLC tags to an HMI tag table

Option 1: Use drag-and-drop to copy tags

  • In the project navigation you first open the HMI tag table into which the PLC tags are to be inserted.
    In this case, the "Default tag table" opens (Fig. 01).


Fig. 01

  • In the project navigation you mark the PLC tag table that contains the PLC tags.
    In this example it is the "Default tag table".
    The "Details view" window shows you the contents of the PLC tags
    (Fig. 02).


Fig. 02

  • In the "Details view" window you mark all the tags to be migrated to the HMI tag table.
  • Drag-and-drop the marked PLC tags into the open
    HMI tag table in the working area.
    Place the "tip" of the cursor in the small gray field next to the "<Add new>" text. A "+" character then appears on the cursor (Fig. 03).


Fig. 03

  • This completes migration of the PLC tags to the HMI tag table (Fig. 04).


Fig. 04

2 Option 2: Use copy-and-paste to copy tags
  • In the project navigation you mark the PLC tag table that contains the PLC tags. In this example it is the "Default tag table".
    The "Details view" window shows you the contents of the PLC tag table (Fig. 05).

Fig. 05
  • In the "Details view" window you mark all the tags to be migrated to the HMI tag table.
  • Right-click the marked tags. A pop-up menu opens. Select the "Copy" item (Fig. 06).


Fig. 06

  • In the project navigation you open the HMI tag table into which the previously copied elements are to be inserted. In this example it is the "Default tag table".
  • Right-click in the small gray field next to the "<Add new>" text. A pop-up menu opens. Select the "Paste" item (Fig. 07).


Fig. 07

  • This completes migration of the PLC tags to the HMI tag table (Fig. 08).


Fig. 08

Table 01

Function description
Migrate elements of a data block to an HMI tag table.
 
No. Function description
1 Migrate elements of a data block to an HMI tag table.

Option 1: Assign tags by drag-and-drop

  • In the project navigation you first open the HMI tag table into which the tags are to be inserted.
    In this example it is the "Default tag table".
  • In the project navigation you open the HMI tag table into which the tags are to be inserted.
    In this example it is the "DB10_HMI_Data" data block.

    Note
    The two windows are displayed as separate Windows windows in the Object bar (Fig. 09).


Fig. 09

  • In each case you mark the complete line of the elements to be migrated
    to the HMI tag table.
  • Click one of the marked labels (Fig. 10) and drag the marked elements to the HMI tag table window. (The window is in the Object bar).
    The HMI tag table window opens.


Fig. 10

  • Drop the elements into the open working area of the HMI tag table. Place the "tip" of the cursor in the small gray field next to the "<Add new>" text.
    A "+" character then appears on the cursor (Fig. 11).


Fig. 11

  • This completes migration of the elements from the data block to the HMI tag table (Fig. 12).


Fig. 12

2

Option 2: Use copy-and-paste to copy tags

  • In the project navigation first you open the data block containing the elements to be migrated to the HMI tag table.
    In this example it is the "DB10_HMI_Data" data block.
    All the elements available to you are displayed in the working area (Fig. 13). 

Fig. 13
  • In each case you mark the complete line of the elements to be migrated to the HMI tag table.
  • Right-click the marked elements. A pop-up menu opens. Select the "Copy" item (Fig. 14).


Fig. 14

  • In the project navigation you open the HMI tag table into which the previously copied elements are to be inserted. In this example it is the "Default tag table".
  • Right-click in the small gray field next to the "<Add new>" text. A pop-up menu opens. Select the "Paste" item (Fig. 15).


Fig. 15

  • This completes migration of the elements from the data block to the
    HMI tag table (Fig. 16).


Fig. 16

Table 02

Keywords
Add tags, Migrate tags, Copy tags

 Entry ID:56045192   Date:2011-11-21 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour