show the entry list
WinCC flexible ES -- Creating HMI configurations -- Creating screens
Why is the script shown in bold type in the PC Runtime although it is not configured as bold type?
How do you create a time switch with WinCC flexible?
How do you create your own on-screen keyboard for a WinCC flexible PC Runtime Station?
How do you register an ActiveX object on the configuration computer and then incorporate it in WinCC flexible?
How do you temporarily lock multiple operator panels?
How do you use a key switch to lock/activate the call of specific screens?
How can you change the tab order in WinCC flexible?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
How can you make a screen selection on a Windows-based operator panel by entering a screen number?
How can you make a screen selection on a Windows-based operator panel via the controller without using a controller job?
How do you configure screen selection on a Windows-based operator panel with WinCC flexible via controller job 51?
How can the display for the danger and warning area of a pointer instrument be made in color?
How do you monitor and control tags on panels on which the status/control object is not available?
Why isn't at the panel the picture number displayed properly in the picture number box after CPU startup?
Multi Panel -- Creating HMI configurations -- Tips and tricks for configuring
How can you write data to a file or read data from a file by means of a script on a Comfort Panel with SIMATIC WinCC (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
With which versions can you select the MP377 15" Touch daylight readable as operator panel?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
Creating underscore with the MP270
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
Touch Panel / Operator Panel -- Creating HMI configurations -- Tips and tricks for configuring
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
Button as pure illuminated indicator with a TP170A
Height of a textbox in a standard configuration (ProTool V6.0)
CPU functions for S7-300 with OP7/OP17
Picture change on the TP170A as tag function
"Tahoma" is the only font that can be used with OP/TP 170A/B and C7-635
How can you implement an OP73 as a handheld?
Mobile Panels -- Creating HMI configurations -- Tips and tricks for configuring
How can you write data to a file or read data from a file by means of a script on a Comfort Panel with SIMATIC WinCC (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
"Clean Screen" function blocked with Mobile Panel 170
Evaluation of the handwheel position on the Mobile Panel 170
What should you pay attention to when configuring a project ID on the Mobile Panel 177 / 277 with battery pack?
How do you create a time switch with WinCC flexible?
Part number:

Description
This FAQ response describes one way you can create a "weekly timer" with WinCC flexible without using program blocks from the PLC.

There are three switching procedures (time intervals) available for each day of the week.
(For example, one for the "early shift", one for the "afternoon shift" and one for the "late shift").
You set the switch-on and switch-off times by way of a "date/time field".

You can select/deselect each switch-on/off time separately.

Once the specified switch-on time is reached, an output signal is set.
This output signal can be transferred to a PLC, to switch on a pump, for example.
Once the specified switch-off time is reached, the output signal is reset.

The following figure shows the Runtime picture created.


Fig. 01

Which operator panels are supported?
The instructions below apply for all operator panels that support scripts. An overview of the functions of the various operator panels is available in Entry ID: 40227286.
In this application we have used an MP 277 Touch.

Please refer to the attached documentation and configuration for details.
The attached download contains a WinCC flexible project with the functions described in the document.

Creation environment
The configuration was made with WinCC flexible 2008 SP2.

Downloads
 
Contents of the downloads

Download

Documentation 
The documentation includes all the necessary configuration steps perform the example in the FAQ.
( 733 KB )
Code 
The packed file contains the sample MP 277 Touch project.
( 2996 KB )

Additional information
 
Title

Link

How do you implement a weekly timer for the SIMATIC S7-1200 in STEP 7 V11? Entry ID: 52722648
S7-300/400 CPUs:
Time switches based on the S7-300/400 CPUs, optional radio clock connection
Entry ID: 21669756

 Entry ID:54997729   Date:2011-11-04 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour