|
Description This entry provides sample programs and documentation for linking IE/AS-i slaves to an S7-300 CPU with integrated PROFINET interface using an IE/AS-i Link.
The sample program consists of a STEP 7 project that contains the configuration of the SIMATIC S7 station and the IE/AS-i Link.
IE_AS-i_Link.zip ( 624 KB )
The document below contains the following:
- An overview of the sample program and plant configuration used to create the sample program.
- Information about installing and commissioning the sample program.
- Information about how to use the sample programs.
- Other notes, tips and tricks, etc.
DP_configuration_IE_AS-i_Link_en.pdf ( 344 KB )
Further Information More information about linking AS-i slaves to a SIMATIC S7 using the IE/AS-i Link is available in the Entry IDs below:
| Description |
Entry ID |
| CPU-CPU Communication with SIMATIC Controllers (Compendium) |
20982954 |
| SIMATIC NET gateway IE/PB Link |
7851748 |
| Manual SIMATIC NET IE/AS-INTERFACE LINK PN IO |
22712154 |
| SIMATIC S7-300 CPU 31xC and CPU 31x: Technical data |
12996906 |
| Automation System SIMATIC S7-400 CPU Specifications |
53385241 |
|