show the entry list
S7-1200 CPU 12xx -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How can the CPU analog inputs of the SIMATIC S7-1200 also measure currents of 0-20mA?
How can you access user-defined web pages of the S7-1200 directly?
How can user-defined web pages and standard web pages be updated automatically in STEP 7 (TIA Portal) V11?
How do you program the "GET" and "PUT" instructions in the user program of the SIMATIC S7-1200 CPU in order to transfer more than 160 bytes of data?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
How in STEP 7 V11 can you access the unstructured data types bit-by-bit, byte-by-byte or word-by-word and symbolically?
How does startup work in an S7-1200?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
How can you prevent data loss of runtime-generated parameters when updating your S7-1200 PLC program?
How can you share runtime-generated parameters between several S7-1200 PLCs with a KTP Basic Panel?
How can you change the IP address of an S7-1200 without using STEP 7 Basic?
How can you delete the IP address and reset your S7-1200 to factory settings using the SIMATIC MC memory card (2MB or 24MB)?
How can you download to a network of several S7-1200 PLCs with the same IP address?
How can you reset the IP address of your S7-1200 PLC using STEP 7 Basic software?
How does startup work in an S7-1200?
Part number:

Description
The startup mode "Warm restart - operating mode before POWER OFF" is set by default in the device configuration. This prevents the CPU from changing unintentionally to the RUN mode during the commissioning phase when the power returns. An unintentional change to the RUN mode will set the outputs and start any machines to which the outputs are connected. However, with this default setting you need a PG with STEP 7 V10.5, STEP 7 V11 or the S7-1200 Tool (see Entry ID 41737437) to be able to change the CPU from STOP mode to RUN mode. The CPU can change to STOP mode for one of the following reasons:

  • Inserting an SD card
  • Failure of an expansion module
  • Other reasons

If STOP mode occurs, you need software for changing to RUN mode.

Remedy
We recommend setting the startup mode "Warm restart – RUN". Then, the CPU changes automatically back into RUN mode when power returns. In this way, neither you nor your customers need customer support’s assistance to set the CPU back into RUN mode.

The table below shows the startup modes of the S7-1200 CPU.
 
Startup mode CPU behavior
No startup CPU remains in STOP mode.
Warm restart – RUN CPU goes into RUN mode when power returns.
Warm restart - operating mode before POWER OFF CPU goes into the same mode as before loss of power.

Note
As from STEP 7 V11 and firmware version V2.0 you have the option of changing operating modes using the web server if activated.
Proceed as follows.

  1. Open the internet browser and start the web server.
  2. Log on as "admin".
  3. Select the "Start page".
  4. Use the "Go to RUN" and "Go to STOP" buttons to change the operating mode accordingly.

 Entry ID:51825007   Date:2011-12-12 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour