show the entry list
ProTool -- Configuring and programming communication -- Configuring communication to S7
Settings in "Status/Force" when using a WinAC MP
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Connecting a ProTool Runtime Panel / PC to an S7 200 via PROFIBUS DP
Connecting a panel to a S7 300/400 controller
Connection settings for a communication between ProTool/Pro and WinAC
How can you increase the performance of HMI devices?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect an operator panel (ProTool) to an H system (S7-400H)?
Connecting a ProTool/Pro Runtime (PC) via Ethernet to an S7-300 or S7-400 station from SIMATIC NET CD 07/2001
ProTool/ProRT and S7-200 with PC/PPI-Cable
Ethernet communication between a ProTool/Pro Runtime (PC) and a CP243-1 (S7-200)
Coupling between ProTool/Pro and WinAC
Coupling between Operator Panel and WinAC Basis/WinAC RTX V4.0
Connection between SIMATIC NET OPC server, ProTool/Pro RT and SIMATIC S7
Connecting an OP as DP slave - configuration of DP direct control buttons
ProTool RT -- Configuring and programming communication -- Configuring communication to S7
PPI connection of ProTool/Pro and S7-200
How do you connect an operator panel (ProTool) to an H system (S7-400H)?
Connecting a panel to a S7 300/400 controller
Ethernet communication between a ProTool/Pro Runtime (PC) and a CP243-1 (S7-200)
Connecting a ProTool Runtime Panel / PC to an S7 200 via PROFIBUS DP
ProTool/ProRT and S7-200 with PC/PPI-Cable
Connecting a ProTool/Pro Runtime (PC) via Ethernet to an S7-300 or S7-400 station from SIMATIC NET CD 07/2001
Coupling between ProTool/Pro and WinAC
Connection between SIMATIC NET OPC server, ProTool/Pro RT and SIMATIC S7
Connecting an OP as DP slave - configuration of DP direct control buttons
Coupling between Operator Panel and WinAC Basis/WinAC RTX V4.0
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
S7-200 CPUs -- Configuring and programming communication -- Configuring communication to PCs
How do you establish a TeleService connection to an S7-200 via a TC65 terminal as remote modem with PIN transfer by PC/PPI cable?
How should you parameterize a GSM modem to set up a connection from an analog modem for teleservicing an S7-200?
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you graphically display a variable of the PLC via EXCEL as OPC client with PC Access as OPC server?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
ProTool/ProRT and S7-200 with PC/PPI-Cable
Why do you get an error message when program downloading in various S7-S7-21x CPUs via USB/PPI or RS-232/ PPI Multi Master cable?
How do you set the network-related parameters for multimaster mode in STEP 7 Micro/WIN?
Which network configuration is typical when implementing the multimaster function?
Which cables do you use for communication in multimaster mode via the COM interface on the PC side?
How can you clear faults in Multimaster mode by parameterizing the COM communications interface on the PC side?
What alternatives are there to connecting to the multimaster network on the PC side?
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
Part number:

QUESTION:
How do you set the correct parameters in Protool/Pro along with the Control Panel to communicate with an S7-200 PLC through Protool/Pro?

ANSWER:
PROCEDURES:
When you create a new Protool/Pro project, you are given a choice of what PLC driver you wish to select. Select the Simatic S7-200 driver as pictured below:

Then click on parameters and the parameters window for the PLC protocol will be displayed as shown below:

Make sure the check box that says Only once Master on the Bus is checked.
You can then close out these dialogue boxes and go into the Windows Control Panel. Double click on Setting the PG/PC interface. For the access point, choose S7Online and for the Interface parameter set used, choose a CP5611(PPI) as shown below. You may have to click the Install button in order to install the CP5611 card.


 Entry ID:5155303   Date:2000-09-28 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour