|
Description Depending on the module and interface through which the connection with the FB65 "TCON" for open communication over Industrial Ethernet is established, you parameterize the "local_device_id" accordingly.
The "local_device_id" for the S7-300 and S7-400 CPUs as well as for the IM151-8 PN/DP CPU and IM154-8 CPU is in the Hardware Configuration (STEP 7 V5.5) or in the Device View of the hardware and network editor (STEP 7 Professional V11). The slot identification for a module's PROFINET interface contains the "local_device_id".
Example for STEP 7 V5.5 The slot identification for the PROFINET interface on a CPU319-3 PN/DP is "X3", in other words you parameterize the "local_device_id" = B#16#03 for open communication through the integrated PROFINET interface on a CPU319-3 PN/DP.

Fig. 01
Example for STEP 7 Professional V11 The slot identification for the PROFINET interface on a CPU319-3 PN/DP is "2 X3", in other words you parameterize the "local_device_id" = B#16#03 for open communication through the integrated PROFINET interface on a CPU319-3 PN/DP.

Fig. 02
Note The slot identification for the PROFINET interface on an S7-300 CPU, S7-400 CPU, IM151-8 PN/DP CPU or IM154-8 CPU is also printed on the module.
Overview The overview below contains the "local_device_ids" which are to be parameterized for open communication by means of WinAC RTX and S7-400 Industrial Ethernet CP. The "local_device_id" of the WinAC RTX depends on the interface slot of the Industrial Ethernet interface.
| local_device_id |
Description |
| B#16#00 |
Communication over Industrial Ethernet CP of the S7-400 (only with ISO-on-TCP, that means connection_type = B#16#12).
Note Entry ID 15368142 contains information about which S7-400 series Industrial Ethernet CPs support open communication services using T blocks. |
| B#16#01 |
Communication through the Industrial Ethernet interface at interface slot 1 (IF1) with WinAC RTX. |
| B#16#06 |
Communication through the Industrial Ethernet interface at interface slot 2 (IF2) with WinAC RTX. |
| B#16#0B |
Communication through the Industrial Ethernet interface at interface slot 3 (IF3) with WinAC RTX. |
| B#16#0F |
Communication through the Industrial Ethernet interface at interface slot 4 (IF4) with WinAC RTX. |
The overview below shows the "local_device_id" designations that you parameterize for open communication through the integrated PROFINET interface of an S7-300 CPU, S7-400 CPU, IM151-8 PN/DP CPU or IM154-8 CPU.
| local_device_id |
Description |
| B#16#01 |
Communication through the integrated PROFINET interface of the IM151-8 PN/DP CPU. |
| B#16#02 |
Communication through the integrated PROFINET interface of the CPU31x-2 PN/DP, CPU314C-2 PN/DP and IM154-8 CPU. |
| B#16#03 |
Communication through the integrated PROFINET interface of the CPU319-3 PN/DP. |
| B#16#05 |
Communication through the integrated PROFINET interface of the CPU412-2 PN, CPU414-3 PN/DP, CPU416-3 PN/DP and CPU41x-5H PN/DP (Rack 0). |
| B#16#15 |
Communication through the integrated PROFINET interface of the CPU 41x-5H PN/DP (Rack 1). |
|