|
QUESTION: Bug fix within Analysis Function ANF OutTCP() of SIPLUS CMS4000 X-Tools Professional V 03.03
During the cyclic sending of TCP/IP telegrams with the Analysis Function ANF OutTCP() the working memory will not be freed again. This can lead to instable behavior of X-Tools depending on telegram size and cycle time during the operating time.
The provided update version fixes this malfunction. This update is released only for SIPLUS CMS4000 X-Tools V 03.03 installations.
ANSWER:
In order to update, please execute the following steps:
1- Download the .zip file ( 13937 KB ) .
2- Unpack the .zip file in a temporary directory.
3- Stop running programs.
4- Create the backup of your existing installation of X-Tools.
5- Remove the write protection from all files of the installation directory:
a. Call the context menu for the installation directory within the Windows Explorer and select “Properties”.
b. Deselect the “Read-only” attribute and press “Apply”.
c. In the upcoming dialog, choose “Apply changes to this folder, subfolders and files” and press “OK”.
6- Start the installation of the new version of X-Tools by launching of “Setup.exe” from the temporary directory.
7- Within the setup, specify the current installation directory of X-Tools as target directory for the ongoing installation.
8- After the setup has been completed, the version is updated. The name of the version and the Configuration Files and settings are unchanged.
|