show the entry list
End of Production for MOBY STG D, MOBY STG I and MOBY STG E RFID Hand Terminals
Part number:
Summary Internet document

Production of the RFID Handheld Service and Test Unit for MOBY D on the basis of the PSION Workabout PRO will be discontinued effective June 30, 2011. The mobile SIMATIC RF310M Hand Terminal for use with ISO 15693 transponders from MOBY D is available as successor product. Production of the RFID reading heads from MOBY D and the PSION Workabout PRO basic unit will also be discontinued.

 

Production of the RFID Handheld Service and Test Unit for MOBY I on the basis of the PSION Workabout PRO, the RFID reading head of MOBY I and the PSION Workabout PRO basic unit, the two RFID Handheld Service and Test Units for MOBY E on the basis of the PSION Workabout PRO/mx and the two RFID reading heads of MOBY E and the PSION Workabout PRO basic unit will be discontinued effective June 30, 2011.

 

 

Internet document Summary
 

Production of the RFID Handheld Service and Test Unit for MOBY D (order no. 6GT2603-0AA10), the RFID reading heads of MOBY D (order no. 6GT2603-1AA00,-1AA10) and the PSION Workabout PRO basic unit (order no. 6GT2003-0AA10) will be discontinued effective June 30, 2011. The products 6GT2603-0AA10 and 6GT2003-0AA10 will cease to be available from this point on, but can still be repaired. Hand terminals are not available on a spare part basis, they can only be repaired on a turnaround basis (same unit back). The reading heads (order no. 6GT2603-1AA00,-1AA10) are available as spare parts without having to return the defective unit.

 

Recommended successor product

The mobile RF310M hand terminal is available for use with ISO 15693 transponders of MOBY D (MDS Dxxx). Older MOBY D data carriers with 44-Byte user memory (6GT2600-0AA00, -0AB00) cannot be used with RF310M. In this case please speak to your contact partner at your local Siemens office.

 
Affected Products Successor Product
Product Name Order No. Product Name Order No.
MOBY D Hand terminal STG D 6GT2603-0AA10 RF300 Hand terminal RF310M 6GT2803-0AB00
MOBY STG x basic unit 6GT2003-0AA10 (not required with RF310M) --
MOBY D reading head 6GT2603-1AA00 (not required with RF310M) --
MOBY D reading head 6GT2603-1AA10 (not required with RF310M) --

 

Production of the RFID Handheld Service and Test Unit for MOBY I (order no. 6GT2003-0CA10) on the basis of the PSION Workabout PRO, the RFID reading head of MOBY I (6GT2003-1CA00) and the PSION Workabout PRO basic unit (6GT2003-0AA10) will be discontinued effective June 30, 2011. The products 6GT2003-0CA10 and 6GT2003-0AA10 will cease to be available from this point on, but can still be repaired. Hand terminals are not available on a spare part basis, they can only be repaired on a turnaround basis (same unit back). The reading heads (order no. 6GT2003-1CA00) are available as spare parts without having to return the defective unit.

 

Successor system

The phase-out for the MOBY I RFID-System was announced on Oct. 01, 2008 (see entry ID: 29825498). The successor system for MOBY I is SIMATIC RF300.

 

 
Affected Products
Product Name Order No.
MOBY I Hand terminal STG I (PRO) 6GT2003-0CA10
MOBY STG x basic unit 6GT2003-0AA10
MOBY I reading head 6GT2003-1CA00

 

Production of the RFID Handheld Service and Test Unit for MOBY E (order no. 6GT2303-0AA10) on the basis of the PSION Workabout PRO, the STG E on the basis of the PSION Workabout mx (6GT2303-0AA00), the RFID reading heads of MOBY E (6GT2303-1AA00,-1AA10), and the PSION Workabout PRO basic unit (6GT2003-0AA10) will be discontinued effective June 30, 2011. The products 6GT2303-0AA00, -0AA10 and 6GT2003-0AA10 will cease to be available from this point on, but can still be repaired. Hand terminals are not available on a spare part basis, they can only be repaired on a turnaround basis (same unit back). The reading heads (order no. 6GT2303-1AA00,-1AA10) are available as spare parts without having to return the defective unit.

 

Successor system

The phase-out for the MOBY E RFID-System was announced on Oct. 01, 2010 (see entry ID: 44466959). The two HF RFID systems SIMATIC RF300 and RF200 are suitable as successors.

 

 
Affected Products
Product Name Order No.
MOBY E Hand terminal STG E (PRO) 6GT2303-0AA10
MOBY E Hand terminal STG E (mx) 6GT2303-0AA00
MOBY STG x basic unit 6GT2003-0AA10
MOBY E reading head 6GT2303-1AA00
MOBY E reading head 6GT2303-1AA10

 

 

 

 Entry ID:50683395   Date:2011-06-08 
I regard this article....as helpfulas not helpful                                 
related links
MOBY STG Hand-Held Terminal for M ...
MOBY STG Hand-Held Terminal PRO, ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour