show the entry list
STEP 7 (TIA Portal) -- Creating S7 programs -- Loading and testing S7 programs
Why in STEP 7 (TIA Portal) V11 is the block comparison different although the networks are the same offline and online?
How do you do a program upload in STEP 7 (TIA Portal) V12 when the device has been configured withSTEP 7 V11?
Why in STEP 7 V11 are the online changes made to technology object parameters marked as retained not effective?
Why are blocks marked differently in the STEP 7 V11 Online View although they are identical?
How should you create a user-defined website in STEP 7 (TIA Portal) in order to control the CPU with an iPad?
How do you load a project into the CPU in STEP 7 (TIA Portal) V11?
In STEP 7 (TIA Portal) V11, how can you upload blocks from the CPU to the PG, for example, into a newly created project?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
Why is communication between the Runtime simulation and the S7-1200 not possible if the PG/PC interface is not set correctly?
How do you transfer a program to an S7-1200 CPU without TIA Portal V11?
How can you have two online connections between STEP 7 V5.5 and an S7-300 and between STEP 7 V11 and an S7-1200 side by side?
In STEP 7 (TIA Portal), how do you download/upload a single data block into/out of the S7-1200 CPU without overwriting the monitored values?
In STEP 7 (TIA Portal), how do you download/upload a single data block into/out of the S7-1200 CPU without overwriting the monitored values?
Part number:

Description
When you upgrade your S7-1200 CPU with firmware V2, after downloading from STEP 7 (TIA Portal) the CPU does a warm restart the first time a change is made to RUN mode. A warm restart does not cause the data in the DBs and the monitoring values to be overwritten with the start values.

S7-1200 CPU modules that still have firmware version V1, are put into STOP mode when downloading from STEP 7 (TIA Portal) even if you are downloading just one block. When the change is then made to RUN mode, the cold start of the CPU deletes all the memory areas including the remanent memory areas and in the data blocks the monitored values are overwritten with the start values.

In this way, with the S7-1200 as from firmware V2 you have the option of downloading the changed data blocks to the CPU without the CPU going into STOP. Only if you put the CPU into STOP and then into RUN mode again will the monitoring values in the main memory be overwritten with the start values. Alternatively you can also overwrite the monitoring values by means of the monitoring table.

However, please note the two cases in which your CPU with firmware V2 nevertheless performs a cold start:

  • When you download the project from STEP 7 V10.5 into a CPU with firmware V2.
  • When you download your program in STEP 7 (TIA Portal) into a CPU with firmware V2, but you have a CPU with V1 configured in the device configuration.

The table below shows the differences between the S7-1200 and the S7-300/400 modules when you download data blocks from a CPU.
 
Action S7-1200 S7-300/400
Storage of the start values with which a DB was downloaded into the CPU In the load memory In the load memory
(values can no longer be read back from the load memory)
After download from the CPU Start values are transferred back again from the load memory into the offline DB The current monitored values are downloaded from the CPU and transferred to the "Start values" column in the offline DB.

Note
You can use the monitored values that the tags are currently capturing in the CPU as start values in the data block. Refer to the information in the STEP 7 (TIA Portal) Online Help under:

  • "Use monitored values as start values"
  • "Download blocks to device in RUN mode (S7-1200/1500)"
  • "Download blocks to device in RUN mode (S7-300/400)"

 Entry ID:50379693   Date:2013-05-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour