|
Description This entry contains sample programs and documentation for communication between a PC station and SIMATIC S7 using S7 communication and incorporating an IE/PB link gateway.
The sample program consists of a STEP 7 project containing the configuration of the SIMATIC S7 station, PC station and IE/PB link, and also consists of an OPC client.
| Active partner PC |
Passive partner S7 |
Sample program with active partner PC |
Sample program with passive partner S7 |
| IE General |
CP343-5 |
OPC_Client.zip ( 12 KB ) |
example_project.zip ( 254 KB ) |
The document below contains
- An overview of the sample program and plant configuration used to create the sample programs
- Information about installing and commissioning the sample program
- Information about how to use the sample programs
- Other notes, tips and tricks, etc.
NET_communication_from_IE_to_PB_via_gateway_en.pdf ( 571 KB )
More information More information about communication between PC station and SIMATIC S7 via network components is available in the entries below.
| Description |
Entry ID |
| What properties, advantages and special features does the S7 protocol offer? |
26483647 |
| S7 CPs for PROFIBUS Configuration and Commissioning |
1158693 |
| Functions (FC) and Function Blocks (FB) for SIMATIC NET S7 CPs Programming Manual |
30564821 |
| CPU-CPU Communication with SIMATIC Controllers (Compendium) |
20982954 |
| SIMATIC NET IE/PB link gateway |
7851748 |
| Network Gateway IE/PB Link PN IO for Industrial Ethernet / Manual Part BL1 |
19299692 |
| SIMATIC NET Industrial Communication with PG/PC Volume 1 - Basics System Manual |
42783968 |
| Industrial Communication with PG/PC Volume 2 - Interfaces Programming Manual |
42783660 |
| SIMATIC NET Industrial Communications Commissioning PC Stations - Manual and Quick Start |
13542666 |
|