show the entry list
WinCC -- Product information -- Checking compatibility
Compatibility Tool for Automation and Drive Technology
Important note on Microsoft Patches KB 943459 and KB 971468
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
How can you find out which Microsoft Patches are installed on the PC?
Further information on the Catalog ST80 with regard to WinCC Communication
Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x?
With which Microsoft Windows operating systems is SIMATIC WinCC/ProAgent compatible?
Which security patch do you need for installing SIMATIC WinCC V6.0?
Drivers on the SIMATIC NET CD 07/2001 and WinCC
Notes on using WinCC V5.1 with "SIMATIC NET 7/2001 SP4"
Microsoft Windows language versions released for SIMATIC WinCC V5.1
WinCC -- Setting up development environments -- Installing and upgrading software
What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?
Why do I receive errors during the upgrade installation to WinCC version V7.0 SP2?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
How can you switch the Microsoft SQL Server Management Studio Express to English on the bundle PC IPC 477C with WinCC V7.0 SP1?
Why does the installation of Microsoft SQL Server 2005 abort?
Why can't you install the SQL server from WinCC V6.2 or WinCC V6.2 SP2 after installing WinCC flexible 2008?
How do you install WinCC V7.0 on a MUI operating system if the language set in Windows is not English?
What can you do if installation of Security Patch KB929046 fails in the Windows Server 2003 R2 SP2?
Why is it not possible to activate the subcomponent "Common" while installing the "Microsoft Message Queuing" component?
How can you install WinCC while the computer is logged on to a domain?
Why does installation of the "Microsoft Message Queuing Services" abort with an error message?
What is the difference between an upgrade and an update?
How do you upgrade the WinCC Options V6.1?
How do you upgrade WinCC V6.0 to WinCC V6.0 SP3?
How do you migrate WinCC V4.x projects to WinCC V6.x and WinCC V7.x?
How can you regularly receive updates to the latest versions of WinCC?
Which settings do you have to make to set up a redundant single-user station in Microsoft Windows XP SP2?
How can you analyze errors when installing WinCC?
Why is the Setup of SIMATIC WinCC aborted at the ACE component (Active Communication Environment)?
How should you proceed if installation of the Microsoft SQL server fails?
Missing SQLUNIRL.dll when Installing SIMATIC WinCC V6
Why does the SQL server 2000 SP3 not appear as present during the installation of WinCC V6.0 SP3, even though it is installed?
WinCC -- Setting up development environments -- Installing / setting up operating systems
Why do other WinCC stations not appear in the network environment on the Windows 7 and Windows Server 2008 PCs?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
What should you watch out for when using WinCC in a domain?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
What should you pay attention to when using WinCC with OEM operating systems?
How do you uninstall SP3 of Microsoft Windows XP?
Detailed information via the installed version of Microsoft Windows
Why can the WinCC uniclient not open the project from the server?
What restrictions are there for assigning the computer name for WinCC?
Logging off USB sticks from the operating system
How can you prevent Microsoft Windows Explorer from being opened as soon as you connect a USB stick to the computer or insert a CD/DVD in a drive?
How can you prevent the "Autoplay" function when inserting a CD/DVD or when connecting a USB device?
ES - SIMATIC Manager -- Product information -- Checking compatibility
Compatibility Tool for Automation and Drive Technology
What are the basic requirements for data exchange between COMOS and SIMATIC PCS 7?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
How can you find out which Microsoft Patches are installed on the PC?
Why can different versions of PCS 7 not be operated in mixed mode?
Which modules and their firmware versions are released for PCS 7 and how can you update them?
With what are SIMATIC PCS 7 V8.x, V7.x, V 6.x, V5.x and V4.x compatible?
Why can't you use Service Packs for Microsoft Windows, the MS SQL Server or the Internet Explorer if they do not originate from the CDs/DVD provided with the PCS 7 software?
What support does Microsoft provide for Microsoft products (operating systems and Internet Explorer) implemented with PCS 7?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC PCS 7?
Important note on Microsoft Patches KB 943459 and KB 971468
Important note when using Microsoft's automatic update service in PCS 7.
Additional information on the compatibility of PCS 7 V6.x and Microsoft products
WinCC (TIA Portal) -- Product information -- Checking compatibility
Compatibility Tool for Automation and Drive Technology
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
Which SIMATIC software can you install in 64-bit operating systems?
Which devices and modules are supported by STEP 7 Professional and WinCC Professional in the TIA Portal?
With what are SIMATIC WinCC (TIA Portal) compatible?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
Part number:

Description
Installation of one of the Microsoft security patches KB2467174, KB2467175, KB2465361 or KB2465367 causes a massive drain on resources (increase in handles) in WinCC Runtime (OS Runtime, WinCC Runtime Professional V11). This consumption of resources can lead to a standstill of WinCC Runtime.
It is strongly recommended not to install any of the Microsoft security patches KB2467174, KB2467175, KB2465361 or KB2465367.

Detailed information about these Microsoft security patches is available at these links:

A remedy is given in the entries below under the corresponding KB numbers.

Note
Refer also to
"Which Microsoft Security Patches have been tested for compatibility with SIMATIC WinCC?" in Entry ID: 18752994 and
"Which Microsoft Security Patches have been tested for compatibility with SIMATIC PCS 7?" in Entry ID: 18490004.

 Entry ID:50197324   Date:2012-06-29