show the entry list
SIMOCRANE Basic Technology
SIMOCRANE: Load change of power semiconductors
SIMOCRANE Basic Technology – Getting Started and Tips for commissioning
SIMOCRANE Basic Technology: Slack rope controller and Current equalization controller
SIMOCRANE Basic Technology: Changes in SIMOCRANE Basic Technology V2.0 SP2
SIMOCRANE Basic Technology: Axis without encoder
SIMOCRANE Basic Technology : Switchover between Trolley and Boom
SIMOCRANE: SIMOTION RT-License
SIMOCRANE: Long delay time between switch off and on with the pulse enable
SIMOCRANE: IPO-overflow
SIMOCRANE: Upgrade Scout and Simocrane application project
SIMOCRANE: Assignment of DP address at DRIVE-CLiQ slots on Simotion D435
SIMOCRANE: DRIVE-CLiQ - clock synchronization
SIMOCRANE: Link to Cranes Application Notes and SIMOCRANE Standard applications and Tools
SIMOCRANE: Application with SINAMICS V2.6 SP2 and SIMOCRANE Basic Technology
SIMOCRANE: Offset-Mode in synchronous operation
SIMOCRANE: Switch over one motor between two drives (Motor Modules)
SIMOCRANE: Set the actual position automatically after Power-On
SIMOCRANE: Output-choke in switch-over one drive between two motors
SIMOCRANE: Problem in Standard project for Overhead Bridge Crane (OHBC)
SIMOCRANE Basic Technology: Failure detection on Active Line module in parallel operation
SIMOCRANE Basic Technology: Axis without encoder
Part number:

FRAGE:
How to configurate an axis without encoder in the standard application?

ANTWORT:

Beispiel: Zwei Gantry-Achsen haben keine Geber.

  1. To delete TO_Gantry_1 and TO_Gantry_2, configurate two TOs with exact the same name, but without check off 'positioning', refer to Manual 10/2010, Chapter 8.13.2.2.
  2. The position-coupling between Gantry 1 und Gantry 2 must be removed:
    • go to program/Gantp_2/gantrymcc_2_s/Operation Mode
    • open Crane_FB_Library.fb_op, you find "to_checkbackmasteraxis" at the line 83 (V2.0 SP1) or the line 82 (V2.0 SP2)
    • delete the content "Gantry_1"
  3. To delete the function 'Referencing' for Gantry
    • go to program /Mon_Ref/referencingmcc_1/
    • delete the Modul 'Gantry'
  4. To set one signal manually to 'True' by doing (Only for V/f control*):
    • go to program/Gantp_1/gantrymcc_1_s/Operation Mode
    • open the program Crane_FB_Library.fb_op, you find "bocheckbackSpeedControllerActive' at line 80 (V2.0 SP1) or at line 79 (V2.0 SP2)
    • setting it as 'TRUE'
    • repeat it to TO_Gantry_2

Reason (Manual 10/2010, P.211, Note):
In the V/f-control the speed controller is not used, as a result the 'speed controller active' signal is not automatically set.

Note:
For configuration of all Gantry DOs it is always required to select the control-mode 'n/M control + V/f control, I/f control', otherwise the drive can’t be controlled by Simotion. It is also possible to select 'V/f control' by Sinamics parameter p1300 later on.

* The 4th step must be only applied, if you use V/f control. If you use sensorless VectorControl [Speed control (sensorless)], then don't change anything, except to configurate the DO without encoder.

 Entry ID:50032136   Date:2011-05-11 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour