show the entry list
SIMOCRANE Basic Technology
SIMOCRANE: Load change of power semiconductors
SIMOCRANE Basic Technology – Getting Started and Tips for commissioning
SIMOCRANE Basic Technology: Slack rope controller and Current equalization controller
SIMOCRANE Basic Technology: Changes in SIMOCRANE Basic Technology V2.0 SP2
SIMOCRANE Basic Technology: Axis without encoder
SIMOCRANE Basic Technology : Switchover between Trolley and Boom
SIMOCRANE: SIMOTION RT-License
SIMOCRANE: Long delay time between switch off and on with the pulse enable
SIMOCRANE: IPO-overflow
SIMOCRANE: Upgrade Scout and Simocrane application project
SIMOCRANE: Assignment of DP address at DRIVE-CLiQ slots on Simotion D435
SIMOCRANE: DRIVE-CLiQ - clock synchronization
SIMOCRANE: Link to Cranes Application Notes and SIMOCRANE Standard applications and Tools
SIMOCRANE: Application with SINAMICS V2.6 SP2 and SIMOCRANE Basic Technology
SIMOCRANE: Offset-Mode in synchronous operation
SIMOCRANE: Switch over one motor between two drives (Motor Modules)
SIMOCRANE: Set the actual position automatically after Power-On
SIMOCRANE: Output-choke in switch-over one drive between two motors
SIMOCRANE: Problem in Standard project for Overhead Bridge Crane (OHBC)
SIMOCRANE Basic Technology: Failure detection on Active Line module in parallel operation
SIMOCRANE Basic Technology : Switchover between Trolley and Boom
Part number:

QUESTION:
How to make sequential control for switchover between trolley and Boom?

ANSWER:

Note:
The sequential control for switchover is different from V2.0 SP1 (also previous versions) to V2.0 SP2.

Trolley > Boom:

Version V2.0 SP1 (also previous versions)

Trolley:

1. Deselect the operation-mode of Trolley: AppSTW1 Bit 10 – 15 = FALSE
2. Check if it is deselected: AppZSW1 Bit 10 – 15 = FALSE
3. Deselect Off1 or Pulse enable: STW1 Bit 0 oder Bit 3 = FALSE
4. Deselect “boChangeTechnologyObject”: AppSTW2 Bit 15 = FALSE
5. Check if it is deselected: AppZSW2 Bit 15 = FALSE
6. Check Trolley drive: ZSW1 Bit 9 = FALSE

 

Boom:

7. Check operation-mode of Boom is deselected: AppZSW1 Bit 10 – 15 = FALSE
8. Select the Technology Object of Boom: AppSTW2 Bit 15 = TRUE
9. Check “boChangeTechnologyObject”: AppZSW2 Bit 15 = TRUE
10. Check Boom drive: ZSW1 Bit 9 = TRUE
11. Select operation-mode of Boom: AppSTW1 Bit 10 – 15
12. Check if operation-mode is selected: AppZSW1 Bit 10 – 15
13. Select Off1 or Pulse enable: STW1 Bit 0 oder Bit 3 = TRUE

Version V2.0 SP2 (NEW) 

Trolley:

1. Pulse disable: STW1 Bit 3 = FALSE
2. Deselect “boChangeTechnologyObject”: Appl_STW2 Bit 15 = FALSE
3. Check Trolley drive: ZSW1 Bit 9 = FALSE

 

Boom:

4. Select “boChangeTechnologyObject”: Appl_STW2 Bit 15 = TRUE
5. Check Boom drive: ZSW1 Bit 9 = TRUE
6. Pulse enable: STW1 Bit 3 = TRUE   

Boom > Trolley:

Version V2.0 SP1 (also previous versions)

Boom:

1. Deselect the operation-mode of Boom: AppSTW1 Bit 10 – 15 = FALSE
2. Check if it is deselected: AppZSW1 Bit 10 – 15 = FALSE
3. Deselect Off1 or Pulse enable: STW1 Bit 0 oder Bit 3 = FALSE
4. Deselect “boChangeTechnologyObject”: AppSTW2 Bit 15 = FALSE
5. Check if it is deselected: AppZSW2 Bit 15 = FALSE
6. Check Boom drive: ZSW1 Bit 9 = FALSE

 

Trolley:

7. Check operation-mode of Trolley is deselected: AppZSW1 Bit 10 – 15 = FALSE
8. Select the Technology Object of Trolley: AppSTW2 Bit 15 = TRUE
9. Check “boChangeTechnologyObject”: AppZSW2 Bit 15 = TRUE
10. Check Trolley drive: ZSW1 Bit 9 = TRUE
11. Select operation-mode of Trolley: AppSTW1 Bit 10 – 15
12. Check if Operation-mode is selected: AppZSW1 Bit 10 – 15
13. Select Off1 or Pulse enable: STW1 Bit 0 oder Bit 3 = TRUE

Version V2.0 SP2 (NEW)

Boom:

1. Deselect pulse enable: STW1 Bit 3 = FALSE
2. Deselect "boChangeTechnologyObject": AppSTW2 Bit 15 = FALSE
3. Check boom drive: ZSW1 Bit 9 = FALSE

 

Trolley:

4. Select "boChangeTechnologyObject": AppStw2 Bit 15 = TRUE
5. Check trolley drive: ZSW1 Bit 9 = TRUE
6. Pulse enable: STW1 Bit 3 = TRUE

 

 Entry ID:50025321   Date:2011-05-09 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour