show the entry list
PROFIBUS general -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
Which options are available for configuring the ET 200 stations?
Configuration of the alarm mode in STEP 7 for the diagnostics repeater (6ES7 972-0AB01-0XA0)
Correction to bus time calculations
Basic knowledge for configuring PROFIBUS-DP networks
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Cyclic program processing only once all the DP stations have signaled that they are finished
Which parameters must be taken into account when planning an electrical network?
How can you calculate the bus cycle time on the PROFIBUS DP with STEP 7?
S7-400 CPU 41x -- Product information -- Background and system information
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function?
Behavior of the CPU after power off without back-up battery
I/O addressing with DP slaves
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What is the difference between a restart (warm restart), cold restart and hot restart of a S7-400 CPU?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
Which entries deal with consistent data in conjunction with distributed I/O?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
What are the requirements for using the S7 routing function and which modules can you implement?
CPU does not work in RUN
What does "Correction factor" mean in the "Diagnostics/Clock" tab of the CPU's Properties dialog?
What is multicomputing mode and what are the differences to operating in the segmented subrack?
Differing information on the requirement of offline/ online memory
How can I get an overview of the S7-400 memory concept?
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
Part number:

Description
There are some process cells that must not be shut down during operation. Using CiR (Configuration in RUN) to make changes to a plant during operation it is possible to make certain changes to the configuration in RUN mode.

When adding components or changing their parameters using CiR (Configuration in Run) the station with the highest PROFIBUS address

  • Must be an S7-compatible DP slave (DPS7 slave).
  • Must not be configured with GSD file.

Otherwise the component added or reparameterized with CiR is not parameterized by the CPU and is therefore not ready for operation although the station supports CiR and the CiR elements are configured.

In the Hardware Configuration you can see whether a DP slave has been configured with GSD file. Double-click the DP slave configured to open the Properties dialog of the DP slave. In the "General" tab the name of the GSD file is displayed if the DP slave has been configured with GSD file.


Fig. 01

This applies for the S7-400 Standard CPUs and PROFINET CPUs up to the firmware versions below:

  • V3.1.4
  • V4.1.1
  • V5.3.1
  • V6.0.2

This applies for the fault-tolerant S7-400 CPUs is you have configured S7-400 as standard system and not H system S7-400H up to the firmware versions below:

  • V3.1.5
  • V4.0.12
  • V4.5.3

Note
Assign a DPS7 slave not configured with GSD file the highest PROFIBUS address.

Further Information
More information about configuring the CiR function (Configuration in Run) is available in the manual "SIMATIC STEP7 V5.5 Modifying the System during Operation via CiR". The manual is available for downloading in Entry ID: 45531308.

 Entry ID:49727145   Date:2011-04-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour