show the entry list
Industrial Ethernet S7-300/400 CPs -- Configuring and programming communication -- Using communication blocks
How do you copy the CFC chart "Modbus" from the sample project for OPEN MODBUS / TCP into your user project?
What is the difference between the initialization and runtime parameters on the blocks for Modbus TCP?
Why is the status value A090 (hex) output for Modbus TCP although you have entered the correct license?
What are the differences between the licensed version and the downloadable demo version of the blocks for Modbus TCP?
Why is the value A083 (hex) output permanently at the STATUS output parameter of the block for Modbus TCP when the ENQ_ENR=true input parameter has been set?
How is data with variable message length transferred via the TCP protocol and received by an S7-300 station via the Industrial Ethernet CP?
How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the UDP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the TCP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the ISO transport protocol?
How do you program the FC10 "AG_CNTRL"?
Which commands (CMD) of the FC10 "AG_CNTRL" are supported by the IE CPs?
How many communication jobs may be used simultaneously in an S7-300 CPU for S7 communication via a CP343-1?
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
Notes on using an instance for multiple connection IDs
Internal call of FC5 (AG_SEND) with FTP client blocks (FC 40-44) for the CP343-1 IT (6GK7 343-1GX11-0XE0)
How do you program the communication blocks FB63 "TSEND", FB64 "TRECV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange by way of the integrated PROFINET interface of a CPU or by way of the CP443-1 Advanced?
How do you program communication blocks FC11 and FC12 for the PROFINET IO device?
Block calls for communications processors in multiple runtime layers
Changing the input parameter of the user blocks "AG_SEND" and "AG_RECV" during the runtime of a job
What should you watch out for if you transfer variables with the data type "REAL" when calling the communication blocks FC5/50 "AG_SEND/AG_LSEND" and FC6/60 "AG_RCV/AG_LRCV"?
What should you pay attention to when using the communication blocks FC53 "AG_SSEND" and FC63 "AG_SRECV"?
What points do you need to remember when calling communication blocks FC5/50 and FC6/60 in the STEP 7 user program of the CPU?
How do you program communication blocks FC11 and FC12 for the PROFINET IO controller?
How can you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information?
How do you program the communication blocks FC50 and FC60?
Error STATUS "0x7000" on function block FC6 / FC60 (AG_SEND) with Send/Receive communication on the S7-400 controller
How do you program the communication blocks FC5 and FC6?
Sample program: S7 communication with the blocks SFB14 ("GET") and SFB15 ("PUT") with S7-400
Sample Program: S7 Communication with blocks FB14 ("GET") und FB15 ("PUT") of the CPU 317-2PN/DP
How do you program communication blocks FB8 "USEND" and FB9 "URCV" for data exchange on the S7-300?
"STATUS = 27" (0x001B) with the loadable S7 communication on the S7-300
How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU?
How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU?
Repeating the "BSEND" job (SFB12) when the "BRCV" block (SFB13) is in the "disabled" state ("EN_R = 0")
PROFIBUS S7-300/400 CPs -- Configuring and programming communication -- Using communication blocks
How do you program the communication blocks FC50 and FC60?
How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU?
How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU?
Which blocks for Modbus TCP can you rename or re-wire when the block numbers of the Mode blocks are already being used in the user program?
How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data?
Where can you find sample programs and documentation for using the PROFIBUS DP protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the free Layer 2 of the FDL protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the FDL protocol?
Where can you find sample programs and documentation for using the PROFIBUS FMS protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules as well as for data communication between SIMATIC S5 modules and PCs?
Notes on using an instance for multiple connection IDs
Processing the data from DP slaves via CP342-5 on CPU31x
Block calls for communications processors in multiple runtime layers
Changing the input parameter of the user blocks "AG_SEND" and "AG_RECV" during the runtime of a job
What should you watch out for if you transfer variables with the data type "REAL" when calling the communication blocks FC5/50 "AG_SEND/AG_LSEND" and FC6/60 "AG_RCV/AG_LRCV"?
How do you program the communication blocks FC5 and FC6?
What properties and special features does S7 Basis Communication offer?
PROFIBUS: diagnostics of S7 connections with STEP 7
Repeating the "BSEND" job (SFB12) when the "BRCV" block (SFB13) is in the "disabled" state ("EN_R = 0")
How do you program communication blocks FB8 "USEND" and FB9 "URCV" for data exchange on the S7-300?
Particularities when assigning parameters of the communication blocks of CP 342 / CP 343
What should you watch out for when upgrading the CP 342-5 or fitting spare parts?
Which version of the function blocks do you need to operate a CP 342-5?
CP 342-5 -- How can you tell that the CP 342-5 has withdrawn from the PROFIBUS?
CP 342-5 -- How do you program data communications when your DP slave only has outputs?
CP 342-5 -- How can you read and write consistent data of a DP slave via the CP 342-5?
How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data?
Part number:

Description
You must call the function blocks below in the S7 program in order to transfer data with the S7-300 via an S7 connection configured in NetPro:

  • FB14 "GET"
  • FB15 "PUT"

Function block FB14 "GET" is for reading data out of the partner CPU and function block FB15 "PUT" is for writing data to the partner CPU.
The S7 connection does not have to be configured on both sides, because the S7 communication via FB14 "GET" and FB15 "PUT" is based on the server-client principle.

Description of the S7 program
This sample program shows how to call the function blocks FB14 "GET" and FB15 "PUT" sequentially in the S7 program of the S7-300 in order to transfer more than 160 bytes of data via an S7 connection.

FB14 "GET" is called three times in a row with the same connection number so that 400 bytes of data can be received.

FB15 "PUT" is called three times in a row with the same connection number so that 240 bytes of data can be sent.

The file below gives a detailed description of the S7 program.

PUT_GET_Sequencer_en.pdf ( 1121 KB )

Download the S7 program
The STEP 7 project contains an S7 program for sequential calling of the function blocks FB14 "GET" and FB15 "PUT" so that the S7-300 can receive 400 bytes and send 240 bytes of data via an S7 connection.

Sequencer.zip ( 41 KB )

Notes

  • If you are using an Industrial Ethernet CP or PROFIBUS CP for data communication via S7 connections in the S7-300 station, then utilize the function blocks FB14 "GET" and FB15 "PUT" from the "SIMATIC_NET_CP" library under "CP 300 > Blocks".
  • If you are using the integrated PROFINET interface of the CPU for data communication via S7 connections, then utilize function blocks FB14 "GET" and FB15 "PUT" from "Standard Library -> Communication Blocks -> Blocks" with the family "CPU_300".
  • Information about configuring an S7 connection for data communication with S7-300 and S7-400 Industrial Ethernet CPs are available in Entry ID: 17628518.
 Entry ID:49450152   Date:2011-07-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour