show the entry list
FM 353, 354, 453 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What must be considered when using the SIMATIC S7 FM354 module with incremental encoder?
What should you watch out for when calling FB POS_CTRL and FB POS_MSRM?
Which function modules (FM) can be used remotely in an ET 200M?
What should you watch out for when parameterizing a digital input for the "Set flying actual value" function in Automatic mode?
How do you assign parameters to an FM354 when using an absolute linear rule?
What does MD38 signify with FM 353?
How can you reduce the positioning times for short distances?
What invokes the procedure program error 0x0801 "Program selection subprogram error"?
How many FM 353s or FM 354s can the communicate with an OP that is connected to the CPU via MPI?
Transferring an NC block (traversing program) by user program to an FM353 / FM354
Aborting an active MDI record of an FM353 or FM354
Behavior of the FM 354 upon signal change at the release input
What should you watch out for when calling FB POS_CTRL and FB POS_MSRM?
Part number:

Description
When called, the function blocks FB POS_CTRL and FB POS_MSRM need an instance data block (DB). The function blocks FB POS_CTRL and FB POS_MSRM are not capable of multi-instance contrary to their display.
Therefore, when you call FB POS_CTRL or FB POS_MSRM for multiple channels/axes, you must create a new instance DB for each channel/axis. This instance is to be transferred for assigning the data to the relevant channel/axis when the block is called.

 Entry ID:49084478   Date:2011-04-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour