show the entry list
ES - SIMATIC Manager -- Product information -- Checking compatibility
Compatibility Tool for Automation and Drive Technology
What are the basic requirements for data exchange between COMOS and SIMATIC PCS 7?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
How can you find out which Microsoft Patches are installed on the PC?
Why can different versions of PCS 7 not be operated in mixed mode?
Which modules and their firmware versions are released for PCS 7 and how can you upgrade them?
With what are SIMATIC PCS 7 V8.x, V7.x, V 6.x, V5.x and V4.x compatible?
Why can't you use Service Packs for Microsoft Windows, the MS SQL Server or the Internet Explorer if they do not originate from the CDs/DVD provided with the PCS 7 software?
What support does Microsoft provide for Microsoft products (operating systems and Internet Explorer) implemented with PCS 7?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC PCS 7?
Important note on Microsoft Patches KB 943459 and KB 971468
Important note when using Microsoft's automatic update service in PCS 7.
Additional information on the compatibility of PCS 7 V6.x and Microsoft products
WinCC -- Product information -- Checking compatibility
Compatibility Tool for Automation and Drive Technology
Important note on Microsoft Patches KB 943459 and KB 971468
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
How can you find out which Microsoft Patches are installed on the PC?
Further information on the Catalog ST80 with regard to WinCC Communication
Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x?
With which Microsoft Windows operating systems is SIMATIC WinCC/ProAgent compatible?
Which security patch do you need for installing SIMATIC WinCC V6.0?
Drivers on the SIMATIC NET CD 07/2001 and WinCC
Notes on using WinCC V5.1 with "SIMATIC NET 7/2001 SP4"
Microsoft Windows language versions released for SIMATIC WinCC V5.1
How can you find out which Microsoft Patches are installed on the PC?
Part number:

Description
Microsoft provides the option by means of WMI for determining which patches are installed.

What is WMI/WMIC?
WMI is the abbreviation for "Windows Management Instrumentation".
WMIC (Windows Management Instrumentation Command Line) extends WMI for operation by way of multiple command line interfaces and batch processing script files.

More information about WMI is available from Microsoft in the internet at
http://www.microsoft.com/austria/technet/articles/wmic.mspx (German)
http://technet.microsoft.com/en-us/library/bb742610.aspx (English)

Procedure
 
No. Procedure
1 In the Windows Start menu you select the "Ausführen" menu item and enter the command "cmd". (German version)
In the Windows Start menu you select the "Run..." menu item and enter the command "cmd". (English version)


Fig. 01

2 In the DOS command window that opens you enter the command below:
wmic qfe list full /format:htable >C:\Temp\hotfixes.htm


Fig. 02

This command creates an HTM list with the installed patches of Microsoft  Windows.

3 Go to the path specified (here C:\Temp) and find the file Hotfixes.htm.
This file contains a list of all the Microsoft Windows patches installed on the SIMATIC PC.


Fig. 03

4 In this list you can find the patches required using the Search command.


Fig. 04

Further information
It is also possible to use Microsoft MBSA (Microsoft Baseline Security Analyzer).
http://technet.microsoft.com/en-us/security/cc184924 (English)
http://technet.microsoft.com/de-de/security/cc184924 (German)

Information about which Microsoft patches are released for WinCC is available in Entry ID: 18752994.

Information about which Microsoft patches are released for PCS 7 is available in Entry ID: 18490004.

Keywords
Hotfix, KB

 Entry ID:48844294   Date:2012-01-20 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour