Description Microsoft provides the option by means of WMI for determining which patches are installed.
What is WMI/WMIC? WMI is the abbreviation for "Windows Management Instrumentation".
WMIC (Windows Management Instrumentation Command Line) extends WMI for operation by way of multiple command line interfaces and batch processing script files.
More information about WMI is available from Microsoft in the internet at
http://www.microsoft.com/austria/technet/articles/wmic.mspx (German)
http://technet.microsoft.com/en-us/library/bb742610.aspx (English)
Procedure
| No. |
Procedure |
| 1 |
In the Windows Start menu you select the "Ausführen" menu item and enter the command "cmd". (German version)
In the Windows Start menu you select the "Run..." menu item and enter the command "cmd". (English version)

Fig. 01
|
| 2 |
In the DOS command window that opens you enter the command below:
wmic qfe list full /format:htable >C:\Temp\hotfixes.htm

Fig. 02
This command creates an HTM list with the installed patches of Microsoft Windows. |
| 3 |
Go to the path specified (here C:\Temp) and find the file Hotfixes.htm.
This file contains a list of all the Microsoft Windows patches installed on the SIMATIC PC.

Fig. 03
|
| 4 |
In this list you can find the patches required using the Search command.

Fig. 04
|
Further information It is also possible to use Microsoft MBSA (Microsoft Baseline Security Analyzer).
http://technet.microsoft.com/en-us/security/cc184924 (English)
http://technet.microsoft.com/de-de/security/cc184924 (German)
Information about which Microsoft patches are released for WinCC is available in Entry ID: 18752994.
Information about which Microsoft patches are released for PCS 7 is available in Entry ID: 18490004.
Keywords Hotfix, KB
|