show the entry list
PROFIBUS S7-300/400 CPs -- Configuring and programming communication -- Using communication blocks
How do you program the communication blocks FC50 and FC60?
How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU?
How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU?
Which blocks for Modbus TCP can you rename or re-wire when the block numbers of the Mode blocks are already being used in the user program?
How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data?
Where can you find sample programs and documentation for using the PROFIBUS DP protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the free Layer 2 of the FDL protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the FDL protocol?
Where can you find sample programs and documentation for using the PROFIBUS FMS protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules as well as for data communication between SIMATIC S5 modules and PCs?
Notes on using an instance for multiple connection IDs
Processing the data from DP slaves via CP342-5 on CPU31x
Block calls for communications processors in multiple runtime layers
Changing the input parameter of the user blocks "AG_SEND" and "AG_RECV" during the runtime of a job
What should you watch out for if you transfer variables with the data type "REAL" when calling the communication blocks FC5/50 "AG_SEND/AG_LSEND" and FC6/60 "AG_RCV/AG_LRCV"?
How do you program the communication blocks FC5 and FC6?
What properties and special features does S7 Basis Communication offer?
PROFIBUS: diagnostics of S7 connections with STEP 7
Repeating the "BSEND" job (SFB12) when the "BRCV" block (SFB13) is in the "disabled" state ("EN_R = 0")
How do you program communication blocks FB8 "USEND" and FB9 "URCV" for data exchange on the S7-300?
Particularities when assigning parameters of the communication blocks of CP 342 / CP 343
What should you watch out for when upgrading the CP 342-5 or fitting spare parts?
Which version of the function blocks do you need to operate a CP 342-5?
CP 342-5 -- How can you tell that the CP 342-5 has withdrawn from the PROFIBUS?
CP 342-5 -- How do you program data communications when your DP slave only has outputs?
CP 342-5 -- How can you read and write consistent data of a DP slave via the CP 342-5?
PROFIBUS S5 CPs and IMs -- Configuring and programming communication -- Using communication blocks
Where can you find sample programs and documentation for using the PROFIBUS DP protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the FDL protocol?
Where can you find sample programs and documentation for using the PROFIBUS FMS protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules as well as for data communication between SIMATIC S5 modules and PCs?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the free Layer 2 of the FDL protocol?
I/O access ET200 with CPU 928
Allocation of the parameter "IMST" in the function block FB192
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the FDL protocol?
Part number:

Description
This entry includes sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules by way of PROFIBUS using the FDL protocol.

In the sample programs below we use the services SEND and RECEIVE of the FDL protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules.
 
Active partner S7 Passive partner S5 Sample program for active partners Sample program for passive partners
CP342-5 AG95U SR_FDL_CP342-5_V20.zip ( 72 KB ) SR_FDL_AG95U_V20.zip ( 1 KB )
CP342-5 CP5431 SR_FDL_CP342-5_V20.zip ( 87 KB ) SR_FDL_CP5431_V20.zip ( 4 KB )
CP343-5 AG95U SR_FDL_CP343-5_V20.zip ( 88 KB ) SR_FDL_AG95U_V20.zip ( 1 KB )
CP343-5 CP5431 SR_FDL_CP343-5_V20.zip ( 88 KB ) SR_FDL_CP5431_V20.zip ( 4 KB )
CP443-5 BASIC AG95U SR_FDL_CP443-5B_V20.zip ( 78 KB ) SR_FDL_AG95U_V20.zip ( 1 KB )
CP443-5 BASIC CP5431 SR_FDL_CP443-5B_V20.zip ( 78 KB ) SR_FDL_CP5431_V20.zip ( 4 KB )
CP443-5 EXTENDED AG95U SR_FDL_CP443-5E_V20.zip ( 88 KB ) SR_FDL_AG95U_V20.zip ( 1 KB )
CP443-5 EXTENDED CP5431 SR_FDL_CP443-5E_V20.zip ( 86 KB ) SR_FDL_CP5431_V20.zip ( 4 KB )

In the sample programs below we use the services SEND and RECEIVE of the FDL protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules. Data communication is by way of a multicast connection, i.e. the active partner sends a message to a group of nodes. Receipt of data is not acknowledged.
 
Active partner S7 Passive partner S5 Sample program for active partners Sample program for passive partners
CP342-5 AG95U MC_FDL_CP342-5_V20.zip ( 111 KB ) MC_FDL_AG95U_V20.zip ( 2 KB )
CP342-5 CP5431 MC_FDL_CP342-5_V20.zip ( 109 KB ) MC_FDL_CP5431_V20.zip ( 6 KB )
CP343-5 AG95U MC_FDL_CP343-5_V20.zip ( 116 KB ) MC_FDL_AG95U_V20.zip ( 2 KB )
CP343-5 CP5431 MC_FDL_CP343-5_V20.zip ( 115 KB ) MC_FDL_CP5431_V20.zip ( 6 KB )
CP443-5 BASIC AG95U MC_FDL_CP443-5B_V20.zip ( 131 KB ) MC_FDL_AG95U_V20.zip ( 2 KB )
CP443-5 BASIC CP5431 MC_FDL_CP443-5B_V20.zip ( 129 KB ) MC_FDL_CP5431_V20.zip ( 6 KB )
CP443-5 EXTENDED AG95U MC_FDL_CP443-5E_V20.zip ( 121 KB ) MC_FDL_AG95U_V20.zip ( 2 KB )
CP443-5 EXTENDED CP5431 MC_FDL_CP443-5E_V20.zip ( 120 KB ) MC_FDL_CP5431_V20.zip ( 6 KB )

The document below contains

  • An overview of the plant configuration used for creating the sample programs.
  • An introduction to the blocks required and their communication structure.
  • Details of the user programs of SIMATIC S5 and SIMATIC S7.
  • Information on how to use the sample programs.
  • Other notes, tips and tricks, etc.

PB_communication_S5_and_S7_FDL_en.pdf ( 394 KB )

Note:
More information about communication with SIMATIC S5 and SIMATIC S7 is available in the Entry IDs below.
 
Entry ID Description
26098555 What properties, advantages and special features does the FDL protocol offer?
17596048 How do you configure an FDL connection between the SIMATIC S5 (CP5431) and SIMATIC S7 via PROFIBUS?
48457189 Where can you find sample programs and documentation for using the PROFIBUS DP protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules?
48066532 Where can you find sample programs and documentation for using the PROFIBUS FMS protocol for data communication between SIMATIC S5 modules and SIMATIC S7 modules as well as for data communication between SIMATIC S5 modules and PCs?
1158693 S7 CPs for PROFIBUS Configuration and Commissioning
1158418 SIMATIC NET NCM S7 for PROFIBUS / FMS Volume 2
1804226 SINEC CP 5430 TF with COM 5430 TF, CP 5431 FMS with COM 5431 FMS
12585718 SINEC CP 5431 FMS with COM 5431 FMS
30564821 Functions (FC) and Function Blocks (FB) for SIMATIC NET S7 CPs Programming Manual
20982954 CPU-CPU Communication with SIMATIC Controllers (Compendium)

 Entry ID:48352979   Date:2011-03-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour