show the entry list
WinCC flexible RT -- Setting up systems -- Configuring software
Why is the script shown in bold type in the PC Runtime although it is not configured as bold type?
How can you optimize the picture change times of WinCC flexible Runtime on a PC with Intel graphics chipset?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you simulate the system keyboard via K or F-keys?
How do you change the date format in WinCC flexible?
How do you temporarily lock multiple operator panels?
How do you use a key switch to lock/activate the call of specific screens?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How do you configure the WinCC Autostart for WinCC flexible Runtime?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
How can you optimize the picture change times of WinCC flexible Runtime on a PC with Intel graphics chipset?
Part number:

Requirements
-
SIMATIC WinCC flexible RT 2004 - 2008 SP2
- Windows XP operating system
- PC or Panel PC with Intel graphics chipset.

Description
The entry describes how to reduce picture change times with multiple dynamic objects and graphics of a WinCC flexible Runtime.

1. Determine the graphics chipset
2. Optimize the video driver

1. Determine the graphics chipset
 
No. Procedure
1 Click the Windows "Start" button and then "Run..." in the Start menu.


Fig. 01

2 Enter the instruction "dxdiag" in the input field and confirm the input with the "OK" button.


Fig. 02

3 Open the "Display" tab in the DirectX Diagnostic Tool window.


Fig. 03

Note
The screenshot shows the example of an Intel graphics chipset.

2. Optimize the video driver
 
No. Procedure
1 Open the Windows "Display Properties" dialog box by right-clicking the Windows Desktop and then "Properties" in the menu.


Fig. 04

2 Open the "Settings" tab and click the "Advanced" button to open the Properties of the driver.


Fig. 05

3 Open the "Troubleshoot" tab and reduce the hardware acceleration by one notch.

Before:


Fig. 06

After:


Fig. 07

Note
The monitor that displays the WinCC flexible Runtime must be connected to the graphics card with Intel graphics chipset.

 Entry ID:48283579   Date:2011-03-07 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour