Description This entry includes sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the ISO transport protocol.
The following services of the ISO transport protocol are used for data transfer:
- SEND and RECEIVE short data blocks
- SEND and RECEIVE long data blocks
SEND and RECEIVE short data blocks Communication from SIMATIC S5 modules to SIMATIC S7 modules is by means of Layer 4 services with data lengths of up to 240 bytes.
SEND and RECEIVE long data blocks Communication from SIMATIC S5 modules to SIMATIC S7 modules is by means of Layer 4 services with data lengths of up to 8192 bytes.
The document below contains
- An overview of the plant configuration used for creating the sample programs.
- An introduction to the blocks required and their communication structure.
- Details of the user programs of SIMATIC S5 and SIMATIC S7.
- Information on how to use the sample programs.
- Other notes, tips and tricks, etc.
47905848_IE_communication_S5_and_S7_en.pdf ( 661 KB )
Note: More information about communication with SIMATIC S5 and SIMATIC S7 is available in the Entry IDs below.
| Entry ID |
Description |
| 47944739 |
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the TCP protocol? |
| 47944603 |
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the UDP protocol? |
| 17661306 |
Commissioning and configuring an ISO transport connection via Industrial Ethernet between SIMATIC S5 and SIMATIC S7 |
| 26582267 |
What properties, advantages and special features does the ISO protocol offer? |
| 12586144 |
SINEC CP 1430 TF with COM 1430 TF Volume 1 of 2 |
| 12585718 |
SINEC CP 1430 TF with COM 1430 TF Volume 2 of 2 |
| 30564821 |
Functions (FC) and Function Blocks (FB) for SIMATIC NET S7 CPs Programming Manual |
|