visualizza l'elenco degli articoli
Industrial Ethernet S7-300/400 CPs -- Configuring and programming communication -- Configuring connections
What should you watch out for when configuring fault-tolerant S7 connections over ISO-on-TCP?
How do you configure an ISO transport connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
How do you configure a UDP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
How do you configure an ISO-on-TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S5, S7 and PC modules in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
How do you send/receive data to/from multiple communication partners via the IE CP of an S7-300 or S7-400 station using the UDP protocol?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection for data communication between an S7-200 and an S7-300 or S7-400 on the Industrial Ethernet?
Establishing a connection from a PC to the S7-400 
What differences are there when configuring S7 connections?
What restrictions are there with Industrial Ethernet CPs when the communications service ISO-on-TCP is being used in parallel via the open TCP/IP communication and the SEND/RECEIVE interface?
What do you have to watch out for, in particular, in the assigning of TSAPs in ISO transport connections and ISO-on-TCP connections?
Procedure and meaning of multicast connections with Industrial Ethernet CPs
How do I set up an ISO connection between a SIMATIC S7 (CP343-1) and a SIMATIC 505 (CP1434) via INDUSTRIAL ETHERNET?
How do you configure the WRITE and FETCH services via Industrial Ethernet (ISO transport connection, ISO-on-TCP connection) for the S7-300/400 with Industrial Ethernet CP343-1 or CP443-1?
Commissioning and Configuring an ISO Transport Connection between the SIMATIC S5 and SIMATIC S7 via Industrial Ethernet
How do you configure a specified and an unspecified S7 connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
Configuring a TCP connection via Ethernet (TCP native) between a SIMATIC S7 and a PC with Socket Interface
How do you configure a TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
How do you configure an ISO-on-TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
Numero di ordinazione:

Instructions
You can use the open communication through ISO-on-TCP connections for data exchange by way of the Industrial Ethernet CPs of S7-300 and S7-400.

Below we describe how to configure an ISO-on-TCP connection for sending and receiving data by way of an Industrial Ethernet CP of S7-300 and S7-400.

ISOonTCP_Connection_en.pdf ( 2121 KB )

The functions below are called in the user program of the CPU for sending and receiving data by way of configured ISO-on-TCP connections.

  • FC5 "AG_SEND" and FC6 "AG_RECV" for the S7-300
  • FC50 "AG_LSEND" and FC60 "AG_LRECV" for the S7-400

The entries below contain sample programs and instructions for programming the above-mentioned functions in the user programs of S7-300 and S7-400: 17853532 and 18513371.

Note
More information on communication over the Industrial Ethernet with S7-300 and S7-400 is available in the entries below.
 
Entry ID Description
26484227 What properties, advantages and special features does the ISO-on-TCP protocol offer?
22385024 How do you configure a TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
47885893 How do you configure a UDP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
47885244 How do you configure an ISO transport connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
29737976 How do you program the communication blocks FB63 "TSEND", FB64 "TRECV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange by way of the integrated PROFINET interface of a CPU or by way of the CP443-1 Advanced?
30564821 Functions (FC) and Function Blocks (FB) for SIMATIC NET S7 CPs Programming Manual

 Articolo con ID:47885440   Data:2011-02-03 
Questo articoloè stato utilenon è stato utile                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
Vai all'articolo
Stampa
Creazione PDF 
Invia l'articolo
QuickLinks
Strumento di compatibilità 
Aiuto
Aiuto on-line
Guided Tour