Instructions You can use the open communication through ISO transport connections for data exchange by way of the Industrial Ethernet CPs of S7-300 and S7-400.
Below we describe how to configure an ISO transport connection for sending and receiving data by way of an Industrial Ethernet CP of S7-300 and S7-400.
ISO_Transport_Connection_en.pdf ( 2309 KB )
The functions below are called in the user program of the CPU for sending and receiving data by way of configured ISO-on-TCP connections.
- FC5 "AG_SEND" and FC6 "AG_RECV" for the S7-300
- FC50 "AG_LSEND" and FC60 "AG_LRECV" for the S7-400
The entries below contain sample programs and instructions for programming the above-mentioned functions in the user programs of S7-300 and S7-400: 17853532 and 18513371.
Note More information on communication over the Industrial Ethernet with S7-300 and S7-400 is available in the entries below.
| Entry ID |
Description |
| 26582267 |
What properties, advantages and special features does the ISO protocol offer? |
| 47885440 |
How do you configure an ISO-on-TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? |
| 22385024 |
How do you configure a TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? |
| 47885893 |
How do you configure a UDP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? |
| 30564821 |
Functions (FC) and Function Blocks (FB) for SIMATIC NET S7 CPs Programming Manual |
|