show the entry list
WinCC flexible ES -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Message indicator continues to be displayed despite counter at zero
How do you start a sound file via a script in the WinCC flexible PC Runtime?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you determine the bit number in WinCC for the "Trigger address", the "Acknowledgement PLC" bit and the "Acknowledgement HMI" bit for creating bit messages?
Which configuration steps have to be taken in SIMOTION SCOUT and WinCC flexible to enable Alarm_S messages and technological alarms to be displayed in WinCC flexible Runtime?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
How do you display messages in WinCC flexible?
How can you evaluate the ACK button on a touch operator panel in WinCC flexible?
How can you have system error messages from a SIMATIC S7-300 / 400 displayed in WinCC flexible?
How do you change and display SIMATIC WinCC flexible system events during configuration?
How can you change the ProTool default alarm window setting in WinCC flexible?
How can I acknowledge alarms in WinCC flexible via the PLC?
Why aren't messages output on the event recorder?
Why isn't the "Message display" shown in the foreground, but is covered by picture objects?
Why are no messages from the S7 diagnostics buffer display in WinCC flexible?
How can you get the diagnostics buffer to be displayed in WinCC flexible?
Which settings need to be made in order to display alarm events after a specified point in time?
How can you create messages with externally preset texts as mass data and process them with Excel in WinCC flexible?
Touch Panel / Operator Panel -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
Two-line messages with S7-PDIAG and OP27/TP27
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
Multi Panel -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
Mobile Panels -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
Basic Panels -- Setting up and parameterizing hardware -- Setting up connections
Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you integrate an HMI operator panel into a local network?
Which connector cables are available for connecting to SIMATIC Panels?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Pushbutton Panels -- Setting up and parameterizing hardware -- Setting up connections
Which connector cables are available for connecting to SIMATIC Panels?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Connecting PPs via PROFIBUS DP with the CP5431
Connection of a Pushbutton Panel to a S7-400H system via Y-Link
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
PP7 / PP17 with MPI on S7 200
WinCC flexible RT -- Setting up systems -- Configuring software
How do you safely terminate WinCC flexible by means of an external application?
Why is the script shown in bold type in the PC Runtime although it is not configured as bold type?
How can you optimize the picture change times of WinCC flexible Runtime on a PC with Intel graphics chipset?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you simulate the system keyboard via K or F-keys?
How do you change the date format in WinCC flexible?
How do you temporarily lock multiple operator panels?
How do you use a key switch to lock/activate the call of specific screens?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How do you configure the WinCC Autostart for WinCC flexible Runtime?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
Sinamics G110 -- Maintenance -- Alerts and Messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
Sinamics G120 -- Maintenance -- Alerts and Messages
SINAMICS G120/G120C (CU 2x0x-2): Fieldbus interface setpoint timeout (F01910)
SINAMICS G120, CU250S-2: Parameterizing the standstill monitoring (F07450).
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Which opportunities are available to acknowledge faults without restarting the inverter or cycling the power?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Is it possible to control the occurrence of the fault F0002 – DC link overvoltage?
For the CU2xy-2 of the SINAMICS G120 with firmware version V4.4, how can the analog inputs be parameterized für 4…20mA with monitoring?
SINAMICS G120 (CU230P-2): Why do I get speed instability or an overspeed trip (F07901) at low speed with a Synchronous motor?
SINAMICS G120: Profibus H-system and Y-link connection with SINAMICS G120 CU230P-2 DP slaves
SINAMICS G120 (CU230P-2): Why Do I See a F1000 Trip on my CU230P-2 via the IOP when I Change Certain Parameters?
I am using an IOP handheld kit with my G120 CU240. When I plug the handheld kit into the G120 PC Connection kit my G120 trips with Safety trips (F1601 \ F1625) or there is no communication, why?
SINAMICS G120, SIMATIC ET200x FC: Can I deactivate the alarm A1699 (forced checking procedure required)?
SINAMICS G120/G120C/G120D/G120P: How can I deactivate the BF-LED (bus error LED)?
SINAMICS G120 (CU 2x0x): Is there a fault list that can be quickly integrated into configuration software for diagnostic purposes?
MICROMASTER4 (MM4), SINAMICS G120 (CU2x0x): When fieldbus communication fails, how can fault F0070 be detected by the drive inverter and further processed?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Why are fault messages F00453 and F0090 present although the encoder module was correctly parameterized?
Why can't I acknowledge fault F0395 "Acceptance test"?
Micromaster 4 -- Maintenance -- Alerts and Messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Why are fault messages F00453 and F0090 present although the encoder module was correctly parameterized?
MICROMASTER4 (MM4), SINAMICS G120 (CU2x0x): When fieldbus communication fails, how can fault F0070 be detected by the drive inverter and further processed?
MICROMASTER 440 (MM4): What is the cause of the fault F0030 on my MM440?
MICROMASTER 4 (MM4): Why does my drive not stop with F0090 when an encoder wire breaks when used in a differential connection?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Is it possible to control the occurrence of the fault F0002 – DC link overvoltage?
MICROMASTER 4 (MM4), SINAMICS G120 (CU240x DP): What are the possible causes of F0070 and how do I avoid them?
MICROMASTER 4 (MM4): The Profibus unit fitted to the MM4 shows a red or orange light. What can cause this?
MICROMASTER 4 (MM440): What is the cause of fault F0022 on the inverter?
MICROMASTER 4 (MM4): What is the cause of the AOP message "LCD BIOS Faulty - Corrupt Data Sets - P---- (Lost)"?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Which opportunities are available to acknowledge faults without restarting the inverter or cycling the power?
MICROMASTER 4 (MM4): What is the cause of the AOP message "No Drive Responding"?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
Part number:

Validity
The downloads below are valid only for SINAMICS firmware up to version V4.4. For SINAMICS firmware version V4.5 onwards the error messages are made available as XML files. Using the SINAMICS-XML parsers you can create csv files from the XML files, which you can then import into your HMI project. The SINAMICS-XML parser is available in Entry ID: 77467239. The XML files ready for downloading are available at this link.

Description
This entry includes the error messages of a frequency converter in the form of a text list. This enables you to display the error messages in plain text on the operator panel.
Information about using text lists is available at the links below.

  • Manual WinCC (TIA Portal): "WinCC Advanced > Visualize processes (Advanced) Configuration > Working with text lists and graphics lists > Working with text lists"
  • Manual WinCC flexible: ""WinCC flexible 2008 > "WinCC flexible Engineering System > Working with WinCC flexible > Text lists"

The tables below provide the error messages as libraries that can be downloaded.

1. Downloads for WinCC (TIA Portal)
 
Firmware SINAMICS S110 SINAMICS S120 SINAMICS G110 SINAMICS G120
V 2.5 SP1
HF3
  ( 709 KB )    
V 2.6 SP1   ( 730 KB )    
V 3.0     ( 484 KB ) ( 484 KB )
V 3.2     ( 488 KB ) ( 486 KB )
V 4.3 ( 638 KB ) ( 638 KB )

 

( 638 KB )
V 4.4 ( 737 KB ) ( 737 KB )   ( 737 KB )
MICROMASTER SINAMICS DCM
( 484 KB ) ( 483 KB )

2. Downloads for WinCC flexible
 
Firmware SINAMICS S110 SINAMICS S120 SINAMICS G110 SINAMICS G120
V 2.5 SP1
HF3
 

( 6466 KB )

   
V 2.6 SP1  

( 6595 KB )

   
V 3.0    

( 3543 KB )

( 3354 KB )
V 3.2    

( 3388 KB )

( 3357 KB )
V 4.3 ( 5597 KB )

( 5352 KB )

 

( 5524 KB )
V 4.4 ( 6988 KB ) ( 5794 KB )   ( 6972 KB )
MICROMASTER SINAMICS DCM
( 3464 KB ) ( 1015 KB )

The libraries are available for downloading in WinCC flexible versions 2007, 2008 and 2008 SP2. If you want to use the libraries in older versions of WinCC flexible too, you must save them in the version concerned in each case. More information about this is available in Entry ID: 33934262.

Note
The libraries are available in German, English (GB and US), French, Spanish, Italian and Chinese.
Define the language you wish to have prior to inserting the library:

  • In WinCC flexible under "Language Settings > Project Languages"

  • In WinCC (TIA Portal) under "Languages & Resources > Project languages"

Additional Information
More related information is available in the Online Support at the links below.
 
Product Direct connection
HMI/Frequency converter
Frequency converter
Error lists for HMI
WinCC flexible 29522676 This entry

Note on security
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information is available in Entry ID: 50203404.

 Entry ID:47520881   Date:2013-11-04