|
Description This entry includes the error messages of a frequency converter in the form of a text list. This enables you to display the error messages in plain text on the operator panel.
Information about using text lists is available at the links below.
- Manual WinCC (TIA Portal): "WinCC Advanced > Visualize processes (Advanced) Configuration > Working with text lists and graphics lists > Working with text lists"
- Manual WinCC flexible: ""WinCC flexible 2008 > "WinCC flexible Engineering System > Working with WinCC flexible > Text lists"
The tables below provide the error messages as libraries that can be downloaded.
1. Downloads for WinCC (TIA Portal)
| MICROMASTER |
SINAMICS DCM |
( 484 KB ) |
( 483 KB ) |
2. Downloads for WinCC flexible
| MICROMASTER |
SINAMICS DCM |
( 3464 KB ) |
( 1015 KB ) |
The libraries are available for downloading in WinCC flexible versions 2007, 2008 and 2008 SP2. If you want to use the libraries in older versions of WinCC flexible too, you must save them in the version concerned in each case. More information about this is available in Entry ID: 33934262.
Note
The libraries are available in German, English (GB and US), French, Spanish, Italian and Chinese.
Define the language you wish to have prior to inserting the library:
Additional Information More related information is available in the Online Support at the links below.
| Product |
Direct connection
HMI/Frequency converter |
Frequency converter
Error lists for HMI |
| WinCC (TIA Portal) |
58522638 |
This entry |
| WinCC flexible |
29522676 |
Note on security The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.
|