show the entry list
AS-Interface master -- Product information -- System description
3RK AS-i General: Determination of I/O addresses of an AS-i slave
Meaning of I/O code and ID, ID1, ID2 code in conjunction with AS-Interface modules
What is the significance of the IP protection classes IP65, IP66, IP67?
Which software do you need for the C7-621 module (with integrated AS interface master)?
ET 200eco -- Product information -- Technical data
Which temperature ranges and environmental conditions apply for the outdoor use of ET 200eco PN?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
What is the significance of the IP protection classes IP65, IP66, IP67?
In what way are ET 200eco and ET 200pro resistant to chemicals?
ET 200pro -- Product information -- Technical data
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
Which CPU can you operate as a PROFINET I device?
What are the requirements for using the S7 routing function and which modules can you implement?
What is the significance of the IP protection classes IP65, IP66, IP67?
Industrial Ethernet network components (wireless) -- Product information -- Technical data
Which devices support the "Power over Ethernet" (PoE) function?
What is the significance of the IP protection classes IP65, IP66, IP67?
Why can't I enter the maximum of 16 characters (128 bits) when entering a WEP encryption string?
ISO-Protocol via iWLAN
What is the significance of the IP protection classes IP65, IP66, IP67?
Part number:

Configuration Notes:
The protection rating indicates how suitable electrical equipment (e.g. devices, lighting, installation material) is for various environmental conditions and also the protection for people against potential dangers when using the equipment.

With regard to suitability for various environments, the systems are divided into relevant IP codes (Ingress Protection codes).

The protection rating is always indicated by the letters IP followed by two digits.
The first digit indicates the degree of protection against contact and solid foreign objects.
The table below explains the meanings of the first digits of the IP code.
 
Digit Protection against body contact Protection against solid foreign objects
0 No protection No protection
1 Protected against large parts of the body
(diameter 50mm)
Large solid foreign objects
(diameter 50mm and greater)
2 Finger protection
(diameter 12mm)
Medium-size solid foreign objects
(diameter 12.5mm and greater, and length up to 80mm)
3 Tools and wires
(diameter 2.5mm and greater)
Small solid foreign objects
(diameter 2.5mm and greater)
4 Tools, wire, and small wires
(diameter 1mm and greater)
Granular solid foreign objects
(diameter 1mm and greater)
5 (K) Wire protection (as IP4), dust-protected Dust deposit (not harmful)
6 (K) Wire protection (as IP4), dust-tight No ingress of dust

The second digit indicates the degree of protection against liquids.
The table below explains the meanings of the second digits of the IP code.
 
Digit Protection against liquids
0 No protection
1 Protected against vertically falling drops of water
2 Protected against direct sprays of water up to 15° from the vertical
3 Protected against direct sprays of water up to 60° from the vertical
4 Protected against water sprayed from all directions, limited ingress permitted
4k Protection against water sprayed from all directions under increased pressure, applies only to road vehicles
5 Protected against low pressure jets of water from all directions
6 Protected against heavy seas or powerful water jets (flooding)
6k Protected against powerful water jets under increased pressure (flooding), applies only to road vehicles
7 Protected against the effects of temporary immersion in water
8 Protected against the effects of continuous immersion in water
9k Protection against high-pressure/steam-jet cleaning, applies only to road vehicles

Note:
Each protection rating is to be considered separately. A high protection rating does not automatically include a lower protection rating.

 Entry ID:4686402   Date:2007-12-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour