|
Task description A SIMATIC RF670-Reader with ethernet interface is to be linked with a SIMATIC S7-1200 controller. With the aid of the RF600-device information from the mobile data memory of the RF6xxT series is read and written. The objective is to reliable identify objects with attached data storage and to make the saved object data available for further process steps. The stored RFID codes of the data storage have to be processable at any time.
Solution The focus is on the library blocks which enable communication between SIMATIC S7-1200 controller and SIMATIC RF670R.
Downloads
| Content of Downloads |
Download |
Library description on the Configuration Example X36 Documentation for the implemented STEP 7 V11 library |
 |
| Library for STEP 7 V11 and configuration file for RF-MANAGER Basic 2010 |
 |
Additional information
| Title |
Link |
| SIMATIC RF670R Function Manual |
Entry ID: 44661579 |
| S7-1200 System Manual |
Entry ID: 36932465 |
| SIMATIC RF600 System Manual |
Entry ID: 22437600 |
| RF-MANAGER Basic 2010 System Manual |
Entry ID: 44474587 |
Security Notice
Caution The functions and solutions described in this article confine themselves to the realization of the automation task predominantly. Please take into account furthermore that corresponding protective measures have to be taken up in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the Internet. Further information can be found under the Content-ID 50203404.
Latest modification Library adapted to STEP 7 V11 as of SP1. Standard IP-addresses of the library adapted to the Factory settings of the RF670R.
Keywords RFID, S7-1200, PLC, identifizieren, Code, ID, XML
|