show the entry list
Update 1 for CFC V7.1 + SP2, integrated in SIMATIC PCS 7 V7.1 + SP2
Part number:

DESCRIPTION:

Update 1 for CFC V7.1 + SP2 which is attached for downloading below is of relevance only for: 

  • CFC V7.1 + SP2, integrated in SIMATIC PCS 7 V7.1 + SP2

Correction

In the case of AS crossing copying of CFC charts with interconnections at the inputs, text references are now created at the inputs again, if these interconnections are not a constituent part of the copy quantity.

Software requirements for the installation:

A precondition for the installation of Update 1 is that CFC V7.1 + SP2 is installed.

Installation

  • Save the download file in a directory of your choice.
  • Extract the files packed therein to another arbitrary directory.
  • Before starting with the installation please close all STEP 7 applications.
  • Select the file "Setup.exe" from the extracted files and start it.
  • Follow the installation prompts.

Important!
Before starting with the installation please read the information provided in the readme file of the download package.
 
Update 1 for CFC V7.1 + SP2,  integrated in SIMATIC PCS 7 V7.1 + SP2,
5 languages (German, English, French, Italian, Spanish)  

 CFC_V71_SP2_Update1_EU.zip ( 4431 KB )

Update 1 for CFC V7.1 + SP2, integrated in SIMATIC PCS 7 V7.1 + SP2 ASIA,
bilingual (English, Chinese)

 CFC_V71_SP2_Update1_CHS.zip ( 3976 KB )

 Entry ID:45947417   Date:2010-10-27 
I regard this article....as helpfulas not helpful                                 
related links
Service Pack 2 for SIMATIC BATCH ...
SIMATIC CFC, SIMATIC VT and SIMAT ...
Update 1 for CFC V7.1 + SP1
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour