show the entry list
Industrial Ethernet S7-300/400 CPs -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What should you watch out for when a MAC address is entered for the PROFINET interface or GBIT interface in the configuration of the Industrial Ethernet CP343-1/CP443-1?
How do you configure a shared device when you are using a CPx43-1 Advanced as PROFINET IO controller and the GBIT interface of the module is networked?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Which Industrial Ethernet CPs support the DHCP Option 12 (Host Name) and how do you configure the DHCP Option 12?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
How do you use an Industrial Ethernet CP or SCALANCE S as a gateway?
How do you disable the "Link Layer Discovery Protocol" function at the ports of an IE CP of S7-300 or S7-400?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
What should you watch out for when operating a CP443-1EX20 V2.0 on a CPU V5.1?
Changing the configuration data of users for CP 343-1 IT and CP 443-1 IT
Loading the configuration via LAN into the IE-CP in "STOP" mode
Special points when setting the LAN medium for Industrial Ethernet CPs
Starting up automation systems with Industrial Ethernet without previous node initiation via MPI
Rejected diagnostics connection via TCP/IP protocol after changing the MAC address
Establishing an online connection to an S7-300/S7-400 CPU through several Ethernet interfaces
What should you pay attention to when formatting the file system in the S7-300 and S7-400 Industrial Ethernet CPs?
What should you watch out for when replacing the CP443-1 (6GK7443-1EX11-0XE0) with a CP443-1 (6GK7443-1EX20-0XE0 V1.0) in STEP 7 V5.4 SP3?
What is the meaning of the configuration option "Activate Web server" with CP443-1 EX20?
Why with CP443-1 Advanced is a different firmware version than the module displayed in the C-PLUG info text in the NCM S7 Diagnostics?
Which options are available for assigning the PROFINET IO controller a new IP address?
How can you configure an S7 CP during runtime?
How do you disable the S7 routing functions?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What should you watch out for when using the function block FB55 "IP_CONFIG" to configure an Industrial Ethernet CP?
Why are some of the newer versions of the names of SIMATIC NET modules not used in the hardware catalog?
Why can't my SIMATIC S7-300 Ethernet CP run as many S7 communication connections as specified?
How does connection multiplexing work and how do you configure it for SIMATIC S7-300 Ethernet CPs?
Industrial Ethernet network components (security) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which firewall rules are to be configured in SCALANCE S if a Virtual Private Network (VPN) is set up over the internet between two SCALANCE Ss and the nodes should also be able to access the internet from the internal network?
How do you use an Industrial Ethernet CP or SCALANCE S as a gateway?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
Which firewall rules do you have to define for SCALANCE S in the Security Configuration Tool to allow data traffic between internal and external networks for a specific IP address area?
How do you configure a VPN tunnel between a PC station and SCALANCE S61x via the Internet with the 2008 edition of SOFTNET Security Client?
What options do I have to insert a C-PLUG or what is the purpose of a C-PLUG?
What are the restrictions when configuring the bandwidth limit of a firewall rule with the Security Configuration Tool V2.1?
Which firewall rules should you configure for SCALANCE S in order to have access to the Internet with the PG/PC via the SCALANCE and router?
How do you configure a VPN tunnel between a PC station with Windows XP SP2 and SCALANCE S61x V2.1 via the Internet with the Microsoft Management Console?
How is a VPN tunnel between two SCALANCE S S 61x modules configured in Routing mode via the Internet?
How do you configure a VPN tunnel between a PC station and SCALANCE S61x V2.1 via the Internet with the SOFTNET Security Client Edition 2005 HF1?
What configuration steps are necessary to forward the coded data packages incoming on the SCALANCE S61x from the VPN tunnel to specific internal nodes only?
How do you use an Industrial Ethernet CP or SCALANCE S as a gateway?
Part number:

Description
With the Industrial Ethernet CPs below it is possible to route messages between the subnets of the PROFINET interface and the gigabit interface.
 
Industrial Ethernet CP Order number
CP343-1 Advanced 6GK7343-1GX30-0XE0
CP443-1 Advanced 6GK7443-1GX20-0XE0

However, the Industrial Ethernet CPs and SCALANCE S do not support router protocols like Router Information Protocol (RIP), for example. This is why it is necessary to make the Industrial Ethernet CP and SCALANCE S known to the nodes that use them as a gateway.

In this example a CP343-1 Advanced (6GK7343-1GX30-0XE0) is used as a gateway in order to access a PC in the plant network using SIMATIC NET Field PG.
The PROFINET interface of the CP343-1 Advanced and the PC connected are components of the plant network and are located in subnet 192.168.0.0.
The gigabit interface of the CP343-1 Advanced and the SIMATIC Field PG connected are in subnet 172.16.0.0.


Fig. 01

If you want to access other subnets with the SIMATIC Field PG via a router or a gateway, then enter the IP address of the router or gateway as default gateway for the LAN (Local Area Network) network connection.

If you access other subnets with the SIMATIC Field PG via multiple routers or gateways, then you define the alternative routes on the SIMATIC Field PG in addition to the default gateway.

In this example the IP address 172.16.85.1 of the router is entered as default gateway for the LAN network connection in order to access the company network with the SIMATIC Field PG. This is why it is necessary to define an alternative route on the SIMATIC Field PG in order to access the plant network via the CP343-1 that acts as gateway.


Fig. 02

Open the "Insert New Connection" dialog via the menu "Insert > New Connection...". Enter the "cmd" command to open the DOS prompt window (see Fig. 04).


Fig. 03

In the DOS prompt window you enter the "route ADD" command to configure a new gateway.


Fig. 04

In this example you configure an additional gateway on the SIMATIC Field PG with the IP address 172.16.85.7. In this example of the CP343-1 Advanced the subnet 192.168.0.0 can be reached via this gateway.
The "route ADD" command is structured accordingly as shown below.
 
Command Destination Subnet mask Gateway
route ADD 192.168.0.0 MASK 255.255.255.0 172.16.85.7

 Entry ID:45632056   Date:2010-11-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour