| No. |
Procedure |
| 1 |
Click "Start > Run" to open the dialog "Run" .
Windows 7 or Windows Server 2008:
Click "Start > All programs > Accessories > Run" to open the dialog "Run". |
| 2 |
Enter the command "cmd" and click "OK". The command prompt opens. |
| 3 |
Enter "C:\Programme\Siemens\WinCC\WebNavigator\Server\bin\WinCCWebconfigurator.exe /deinstall=yes" and press ENTER. After you press ENTER the window "Wait" opens. The text "User and Group Settings" is displayed in this window.
Note:
If you didn't use the default path for the installation, you have to change the path accordingly. If you use a MUI or english Version of the operating system you must input the execute within apostrophes. It is necessary the system to recognize the path "Program files". The parameter "/deinstall=yes" must be set external of the apostrophes.
Example: "C:\Program files\Siemens\WinCC\WebNavigator\Server\bin\WinCCWebconfigurator.exe" /deinstall=yes |
| 4 |
Close the command console interpreter. |
| 5 |
Click "Start > SIMATIC > WinCC > Webnavigator Server > Webconfigurator" to open the Webconfigurator and configure the Website. Detailled informations you can find in the WinCC Information System following the path: "Options > WinCC/WebNavigator > WinCC/WebNavigator documentation > Configuring the WebNavigator Server > Setting up the Web Folder". |
| 6 |
Connect the Web client with the Web server. |