Instructions The picture objects in WinCC flexible below support changing of the column width:
- Alarm View
- Message Window
- Recipe Display
- User Display
- Trend Display
- Status/Control Display
- Detail View (ProAgent)
- Step Display (ProAgent)
- Unit Display (ProAgent)
The default values for the column width are predefined for the picture objects given above. You have two options for changing the column width.
- Change the column width in WinCC flexible Runtime
You can drag the column widths of the picture objects to be larger or smaller during WinCC flexible Runtime. The settings made are not stored permanently. The default column width values for the picture objects are reset when you restart WinCC flexible Runtime.
- Change the column width during configuration of the picture object in WinCC flexible
You can change the column width when configuring the picture object in WinCC flexible ES. Open the picture with the configured alarm display, for example. Mark the alarm display with the mouse.

Fig. 1: Marked alarm display
Press and hold the SHIFT key and double-click on the alarm display. The mouse pointer changes and you can now change the column width in the alarm display by dragging the columns to be larger or smaller. The settings are stored permanently for this alarm display.
Keywords
Table, Table of values, Column layout
|