show the entry list
WinCC flexible ES -- Working with projects -- Creating, editing, archiving and copying projects
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How can you change the column width of picture objects in WinCC flexible?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
What are the solutions offered for working with different versions of WinCC flexible?
Which problems might arise if the "log.LDF" file is not available in a WinCC flexible project?
Why does WinCC flexible close again automatically after the program start?
How can you save WinCC flexible projects / libraries as projects / libraries in the format of an earlier version of WinCC flexible?
How can you delete unused tags or objects from a WinCC flexible project?
What options do you have for copying pictures from one WinCC flexible project to another?
Copying HMI projects integrated in SIMATIC STEP 7 at file level
How can you open a WinCC project integrated in STEP 7 faster?
How do you archive projects in WinCC flexible and which files are required?
How do you back transfer the projects of an operator panel and what should you watch out for?
What transfer options are available in the various operator panels?
How can you change the column width of picture objects in WinCC flexible?
Part number:

Instructions
The picture objects in WinCC flexible below support changing of the column width:

  • Alarm View
  • Message Window
  • Recipe Display
  • User Display
  • Trend Display
  • Status/Control Display
  • Detail View (ProAgent)
  • Step Display (ProAgent)
  • Unit Display (ProAgent)

The default values for the column width are predefined for the picture objects given above. You have two options for changing the column width.

  1. Change the column width in WinCC flexible Runtime
    You can drag the column widths of the picture objects to be larger or smaller during WinCC flexible Runtime. The settings made are not stored permanently. The default column width values for the picture objects are reset when you restart WinCC flexible Runtime.
     
  2. Change the column width during configuration of the picture object in WinCC flexible
    You can change the column width when configuring the picture object in WinCC flexible ES. Open the picture with the configured alarm display, for example. Mark the alarm display with the mouse.


    Fig. 1: Marked alarm display

    Press and hold the SHIFT key and double-click on the alarm display. The mouse pointer changes and you can now change the column width in the alarm display by dragging the columns to be larger or smaller. The settings are stored permanently for this alarm display.

Keywords
Table, Table of values, Column layout

 Entry ID:45056973   Date:2010-10-12 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour