show the entry list
Industrial Ethernet network components (electrical/optical) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Where can you find sample programs and documentation for communication between a PC station and SIMATIC S7 via Industrial Ethernet and incorporating network components?
Which GSDML file can you use with the firmware version installed in SCALANCE X?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
Which settings have to be complied with in a PROFINET RT network in conjunction with VLAN switches?
Routing of S7 and of Data Sets (PROFIBUS DP) via the Link Gateway IE/PB
How do you transmit the diagnostics data of an OSM, ESM or SCALANCE to the TFTP server using the Trivial File Transfer Protocol (TFTP)?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
Login window of the "Web Based Management" remains permanently active
What options do I have to insert a C-PLUG or what is the purpose of a C-PLUG?
Which Industrial Ethernet switches can be operated as redundancy managers and which as standby managers in a ring?
How do you transmit the diagnostics data of an OSM, ESM or SCALANCE to the TFTP server using the Trivial File Transfer Protocol (TFTP)?
Part number:

Description
The Trivial File Transfer Protocol (TFTP) is a very simple file transfer protocol. TFTP is a very simplified version of the File Transfer Protocol (FTP) and is a packet-oriented protocol that supports only reading or writing of files. TFTP does not support listing of directory contents, authentication, compression or encryption, for example. The maximum file size is 32 MB with a defined packet size of 512 bytes.

The diagnostics data of the OSM, ESM and SCALANCE network components can be read out by a TFTP server using the Trivial File Transfer Protocol. Proceed using the following instructions:

Settings in the web-based management of network components OSM, ESM and SCALANCE
Make the settings below in the web-based management of the network components.
 

Setting

Description
TFTP Server IP Address IP address of the TFTP server
Configuration File Name of the configuration file (user-definable)
Log Table File Name of the protocol file (user-definable)
Firmware File Name of the firmware file (user-definable)

In the web-based management of SCALANCE X-200, SCALANCE X-300 and SCALANCE X-400 you make the settings in the "System > Save & Load TFTP" menu.

In the web-based management of OSM and ESM you make the settings in the "System > Save & Load" menu.

Settings of the TFTP server
In this example we use the TFTP server "TFTPD32". A sample setting is explained for this TFTP server.
 
No. Procedure
1 Start the TFTP server "TFTPD32" with "tftp32.exe".
2 Make the following settings in the main window:
  • For "Current Directory" you select the directory in which the files are stored.
  • For "Server Interface" you select the network interface via which the TFTP server can be reached.


Fig. 01

3 In the main window you click on the "Settings" button to open the "Settings" dialog and make and verify other settings.


Fig. 02

In the "Settings" dialog you enable or disable the functions below under "Global Settings".
 
Function Status Description
TFTP Server Enabled This function enables/disables the TFTP server.
TFTP Client Enabled This function enables/disables the TFTP client.
Syslog Server Enabled This function enables/disables the system protocol server.
SNTP Server Disabled This function enables/disables the SNTP server.
DHCP Server Disabled This function enables/disables the DHCP server.

In the "Settings" dialog you select the "Standard" option under "TFTP Security". This setting permits read and write access to the directory selected in the main window.

In the "Settings" dialog you make the settings below under "TFTP configuration".
 
Setting Value Description
Timeout (seconds) 3 Maximum timeout between two retransmissions.
Max. Retransmit 6 Maximum number of retransmissions.
tftp port 69 Number of port on which incoming transfers are listened for.
local ports pool - Pool of local ports that may be used for data transfers (connection requests to Port 69 are answered on ports randomly selected by the sender (=TID)). Notation 10000:19999)

In the "Settings" dialog you enable the functions below under "Global Settings".
 
Function Status Description
Negotiation option Enabled The function permits data blocks greater than 512 bytes to be negotiated by server and client (for better performance).
Show Progress bar Enabled When the function is enabled, a progress bar is displayed during file transfer.
Translate Unix file names Enabled The function translates the Unix file separator "/" into "\".

Sending the diagnostics data to the TFTP server
In order to send the diagnostics data to the TFTP server, in the web-based management of SCALANCE X-200, SCALANCE X-300 and SCALANCE X-400 you select the menu "System > Save & Load TFTP". Then click on the "Save Log Table" button.

In the web-based management of OSM and ESM you select the menu "System > Save & Load" and click on the "Save Log Table" button to send the diagnostics data to the TFTP server.


Fig. 03

Note
With SCALANCE you can also use the Hypertext Transfer Protocol (HTTP) to save event logs. In this case it is not necessary to install an TFTP server on the computer.

 Entry ID:44901238   Date:2010-09-20 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour