show the entry list
OS - WinCC -- Operation and maintenance -- Evaluating diagnostics files
How do you use the "SIMATIC Diagnostics Tool" (SDT2012) to collect diagnostics and system data?
How do you use the "SIMATIC Diagnostics Tool" (SDT2011) to gather together the diagnostics and system information of multiple computers on one computer?
Message: Message overflow detected
Why, with SIMATIC PCS 7 basic stations of the types IL 40 and IL 40 S, are there sometimes timeout entries in the Event Log of the Windows operating system?
WinCC -- Operation and maintenance -- Diagnosing errors (evaluating diagnostics files)
How do you use the "SIMATIC Diagnostics Tool" (SDT2012) to collect diagnostics and system data?
How do you perform comprehensive diagnostics in PCS 7 and WinCC plants?
How do you use the "SIMATIC Diagnostics Tool" (SDT2011) to gather together the diagnostics and system information of multiple computers on one computer?
What do the error messages "Transfer buffer too small", "TagQueue overflow" and "Messages are lost" mean?
Why does the error "S7OPCIAX" occur in the event display?
How can you recognize resource bottlenecks in advance from WinCC and react to them accordingly?
Where can you find a description of the error messages of the Global Script diagnostics window in WinCC RT?
How can I determine the name of an action via the error message "Execute Error in Action @xxx"?
What can be the cause of the WinCC error message "More than 10000 actions in work" (up to V6.2: "More than 5000 actions in work")?
How can you back up the data of the Windows event viewer?
How do you save the diagnostics data of the Windows system monitor (performance monitor) in a file?
How can you define the amount of memory required for the performance indicator log of the Windows system monitor (performance monitor)?
Where can I find explanations of the error messages of the WinCC diagnostics files License.log, WinCC_SStart_xx.log and WinCC_Sys_xx.log ?
How do you evaluate and remedy "OnErrorExecute"-type configuration errors?
How do you write outputs from the "APDiag" diagnostic tool to a file?
How do you use the diagnostic tool "APDiag" to debug C scripts?
How do you determine the function name from the function ID in the case of APDiag-OnErrorExecute messages?
How do you start the "APDiag" script diagnostics tool?
WinCC flexible ES -- Operation and maintenance -- Diagnosing errors
How do you use the "SIMATIC Diagnostics Tool" (SDT2012) to collect diagnostics and system data?
How do you use the "SIMATIC Diagnostics Tool" (SDT2011) to gather together the diagnostics and system information of multiple computers on one computer?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
STEP 7 -- Analyzing error messages -- Diagnosing errors
How do you use the "SIMATIC Diagnostics Tool" (SDT2012) to collect diagnostics and system data?
How do you use the "SIMATIC Diagnostics Tool" (SDT2011) to gather together the diagnostics and system information of multiple computers on one computer?
Information about the topic of "Diagnosing errors"
How can you clear the error message 257:5 in STEP 7?
How can you clear the error message "Abnormal Program Termination"?
What is the meaning of the error codes (xxxx:yyyy) in STEP 7?
How do you clear message 256:26 "An OLE error has occurred"?
How do Diagnostics and Remedy work in STEP 7 when an online connection with the CP5511 is not possible?
What is the remedy for error message 13:76?
Why does the area length error warning appear in STEP 7 V5.5 with indirect addressing or when using FC100 "SWR_START"?
Why does the message "S7tgtopx.exe has caused an error and will be closed" appear?
What is the meaning of the error codes (like W#16#8081) of the return value RET_VAL in STEP 7 V5.5?
WinCC (TIA Portal) -- Operation and maintenance -- Diagnosing errors
How do you use the "SIMATIC Diagnostics Tool" (SDT2011) to gather together the diagnostics and system information of multiple computers on one computer?
How do you use the "SIMATIC Diagnostics Tool" (SDT2012) to collect diagnostics and system data?
In WinCC (TIA Portal) how do you calculate the correct error line in a VB script for the WinCC Professional Runtime?
STEP 7 (TIA Portal) -- Operation and maintenance -- Diagnosing errors
What is the meaning of this error message: " Internal system error (error code: 0x8000af6000000011) – Please contact SIMATIC Customer Support."?
How do you use the "SIMATIC Diagnostics Tool" (SDT2011) to gather together the diagnostics and system information of multiple computers on one computer?
How do you use the "SIMATIC Diagnostics Tool" (SDT2012) to collect diagnostics and system data?
In STEP 7 V11, how can you read out the module status information for the S7-1200?
What is a possible remedy in STEP 7 V11 when the error message is display indicating that the PROFINET interface does not have enough modules?
How do you proceed when peripheral device errors are detected by the S7-1200?
How do you use the "SIMATIC Diagnostics Tool" (SDT2011) to gather together the diagnostics and system information of multiple computers on one computer?
Part number:

Introduction
The "SIMATIC Diagnostics Tool" enables you to gather together diagnostics and system information.
The "SIMATIC Diagnostics Tool" acquires the information from a local computer and also from multiple computers by means of remote access over the network.

Description
Scope of functions of the "SIMATIC Diagnostics Tool":

  • Acquisition of diagnostics data.
  • Acquisition of system data.
  • Archiving of acquired information sorted according to computer in the ZIP format.

The tool has two components: "Settings Manager.exe" and "SIMATIC Diagnostics Tool.exe".

  • The Settings Manager is used to configure the information to be acquired.
    • Which diagnostics files?
    • Which system information?
    • From which computers is this information required?
       
  • The Settings Manager creates a configuration file with the inputs.

Advantages of using the "SIMATIC Diagnostics Tool Edition 2011"

  • You do not have to install the tool.
  • You do not have to acquire the information manually from each computer; a "click" is all that is needed.
  • The configuration files of the tool only have to be created once and can be used over again if the identical files have to be acquired at another point in time.
  • You can generate the configuration files "offline" and then forward them to the staff on site. This saves having to make any further settings in the customer plant.
  • The information from all the computers is available on one computer when the tool has completed its run.

New features in SDT2011

  • Gathering of more diagnostics, for example, TIA Portal, .hdmp and .mdmp files, scalance information
  • Support of 64-bit systems (see note below)
  • User-specific profile types and comments

Software requirements
Operating system: Windows 2000, WinXP, Windows 2003 Server, Windows 2008 Server, Windows Vista

  Attachment 1: SDT2011_3.zip ( 3952 KB )

Note
The "SIMATIC Diagnostics Tool Edition 2012" is in Entry ID 65976201.

Instructions
 
No. Procedure
1 Download the Zip file "SDTyyyy_x.zip" from this page to your Engineering Station and unpack the Zip file on your drive, "D:\SDT", for example. Use this password for decoding: "12345678".
2 Download the file "psexec.exe" (psTools) from the Microsoft internet site http://technet.microsoft.com/en-us/sysinternals/bb897553.aspx and copy the file into the subfolder "...\bin".
3 Download the "Userdump" tool from the Microsoft internet site http://www.microsoft.com/downloads/details.aspx?FamilyID=E089CA41-6A87-40C8-BF69-28AC08570B7E and start the self-extracting file. Retain the path and click "Unzip" (see note).
4 Start the SIMATIC Diagnostics Tool and configure as required.

Basic configuration of the SIMATIC Diagnostics Tool
Instructions for the basic configuration

  Basic_Config_SDT_en.pdf ( 444 KB )

Configuration files for local and remote stations

general-configs.zip ( 1 KB )

Note on McAfee Application Control
When using McAfee Application Control, the participating systems must be in Update mode.
This can be run from the central McAfee Server (ePO).
For configurations without a central server, you must make changes on the participating systems. For this, please get in touch with Technical Support.

Note on the Userdump Tool
In the case of 32-bit systems, you must copy the userdump.exe + dbghelp.dll files from the ...kktools\x86 folder into the ...\bin folder.
In the case of 64-bit systems, you must copy the userdump.exe + dbghelp.dll files from the ...kktools\x64 folder into the ...\bin folder.

Note on 64-bit systems
The project export function (reading out diagnostics data from STEP 7 projects and modules) is not available.

Additional Keywords
Log files, Log file, Diagnostics data, Hotline request, WinCC, PCS 7, Analysis, Troubleshooting, Diagnostics file

 

 Entry ID:44029135   Date:2013-01-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour