show the entry list
SIMOCRANE Basic Technology
SIMOCRANE: Load change of power semiconductors
SIMOCRANE Basic Technology – Getting Started and Tips for commissioning
SIMOCRANE Basic Technology: Slack rope controller and Current equalization controller
SIMOCRANE Basic Technology: Changes in SIMOCRANE Basic Technology V2.0 SP2
SIMOCRANE Basic Technology: Axis without encoder
SIMOCRANE Basic Technology : Switchover between Trolley and Boom
SIMOCRANE: SIMOTION RT-License
SIMOCRANE: Long delay time between switch off and on with the pulse enable
SIMOCRANE: IPO-overflow
SIMOCRANE: Upgrade Scout and Simocrane application project
SIMOCRANE: Assignment of DP address at DRIVE-CLiQ slots on Simotion D435
SIMOCRANE: DRIVE-CLiQ - clock synchronization
SIMOCRANE: Link to Cranes Application Notes and SIMOCRANE Standard applications and Tools
SIMOCRANE: Application with SINAMICS V2.6 SP2 and SIMOCRANE Basic Technology
SIMOCRANE: Offset-Mode in synchronous operation
SIMOCRANE: Switch over one motor between two drives (Motor Modules)
SIMOCRANE: Set the actual position automatically after Power-On
SIMOCRANE: Output-choke in switch-over one drive between two motors
SIMOCRANE: Problem in Standard project for Overhead Bridge Crane (OHBC)
SIMOCRANE Basic Technology: Failure detection on Active Line module in parallel operation
SIMOCRANE: Problem in Standard project for Overhead Bridge Crane (OHBC)
Part number:

Question:
How to complete the project?

Answer:
The missed MCC calls can be copied from the standard project for STS. This means that the SIMOTION Scout must be opened two times and the following programs must be copied from the STS standard project to the OHBC standard project: Gantp_1, Gantp_2, Trollp_1, Trollp_2 and Mon_Ref

A complete standard project for OHBC can be downloaded in following.

SIMOCRANE_BasicTechnologyApplication_OHBC.zip ( 2926 KB )

 Entry ID:43999385   Date:2010-07-26 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour