show the entry list
WinCC flexible ES -- Product information -- General information
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How do you make printouts on different printers in WinCC flexible PC Runtime?
How can you exchange data between USB storage devices on the Thin Client with an active RDP connection?
What are the functional differences between the different SIMATIC panels?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make products comply with FDA regulations?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How do you send customer projects to Technical Support?
Why are PDF documents not displayed properly on the MP377?
Which GSD files are there for the Profibus DP operator panels?
Which GSDML files are there for the operator panels for Profinet IO?
Is there a Siemens contact for customer-specific software solutions, extensions to WinCC flexible or own applications for Windows CE Panels?
Thin Client -- Operation and maintenance -- Diagnosing errors
How can you exchange data between USB storage devices on the Thin Client with an active RDP connection?
Is the RDP-USB storage device mapping supported by Windows 7?
When searching for Thin Clients with the Remote Configuration Center Base Edition V1.0, why are not all the Thin Clients in the network displayed?
How can you exchange data between USB storage devices on the Thin Client with an active RDP connection?
Part number:

Description
If there are multiple USB sticks connected to a Thin Client with an RDP connection established, it is not possible to copy or move files directly from one USB stick to another.
 
This behavior applies for the RDP connection between a Thin Client and the operating systems below:
Windows XP SP3
Windows 2003
Windows 2008

Remedy
Store the files first on the Windows Desktop. Then you can move or copy the files to the USB sticks.

 Entry ID:43502448   Date:2010-08-16 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour