Description If there are multiple USB sticks connected to a Thin Client with an RDP connection established, it is not possible to copy or move files directly from one USB stick to another.
| This behavior applies for the RDP connection between a Thin Client and the operating systems below: |
| Windows XP SP3 |
| Windows 2003 |
| Windows 2008 |
Remedy Store the files first on the Windows Desktop. Then you can move or copy the files to the USB sticks.
|