Up until SIMATIC NET CD V8.0 the real data type is only released for high-performance in-process variants of the SIMATIC NET S7 OPC server. This constraint is revoked as of SIMATIC NET CD 2010 (V8.0).
The existing constraint (refer to contribution 38427115 for more details) is revoked as of SIMATIC NET CD 2010 (V8.0).
Details of the SIMATIC NET CD version 2010 (V8.0) can be found under contribution number 43264686.