Description The maximum number of parameters for a function (FC) in an S7-300 CPU is limited to 127. These can be IN, OUT or IN_OUT parameters. On the other hand, the number of parameters for a function block (FB) in an S7-300 CPU is not limited to a specific number, but is restricted by the maximum size of the instance data block.
|