visualizza l'elenco degli articoli
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
Basic Panels -- Creating HMI configurations -- Tips and tricks for configuring
In WinCC V11 (TIA Portal) with Basic Panels how do you configure a connection to communication partners that you can change in runtime?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
Touch Panel / Operator Panel -- Creating HMI configurations -- Tips and tricks for configuring
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
Button as pure illuminated indicator with a TP170A
Height of a textbox in a standard configuration (ProTool V6.0)
CPU functions for S7-300 with OP7/OP17
Picture change on the TP170A as tag function
"Tahoma" is the only font that can be used with OP/TP 170A/B and C7-635
How can you implement an OP73 as a handheld?
Multi Panel -- Creating HMI configurations -- Tips and tricks for configuring
How can you write data to a file or read data from a file by means of a script on a Comfort Panel with SIMATIC WinCC (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
With which versions can you select the MP377 15" Touch daylight readable as operator panel?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
Creating underscore with the MP270
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
Mobile Panels -- Creating HMI configurations -- Tips and tricks for configuring
How can you write data to a file or read data from a file by means of a script on a Comfort Panel with SIMATIC WinCC (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
"Clean Screen" function blocked with Mobile Panel 170
Evaluation of the handwheel position on the Mobile Panel 170
What should you pay attention to when configuring a project ID on the Mobile Panel 177 / 277 with battery pack?
WinCC flexible RT -- Configuring and programming communication -- Configuring communication to S7
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
S7-300 CPU 31x -- Configuring and programming communication -- Configuring the PROFIBUS interface
How do you activate the "Prioritized OCM communication" function to improve the OP communication performance?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
Transfer of analog values from and to the PROFIBUS DP slave
What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
What are the differences between the integrated DP interface of a CPU (e.g. CPU 315-2 DP) and the DP interface of the CP 342-5?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
What are the options for exchanging data between CPUs via MPI/PROFIBUS DP?
Direct data exchange (internode communication) between two CPU modules
S7 routing via PROFIBUS with S7-300
Rules for accessing the CPU 315-2 DP on distributed I/O (integrated DP interface of CPU 315-2 DP)
Startup of the S7-300 CPUs when slave is not available
Routing with compact CPU and C7-635 as DP slave
How can you tell whether your S7-300/400 master supports DPV1 functions?
S7-400 CPU 41x -- Configuring and programming communication -- Configuring the PROFIBUS interface
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
What do you have to consider when connecting a S7-400 CPU to an external master as DP slave?
What differences are there when configuring S7 connections?
Transfer of analog values from and to the PROFIBUS DP slave
What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
How can you tell whether your S7-300/400 master supports DPV1 functions?
Where are the settings of the MPI and PROFIBUS interfaces retained after updating the operating system for a CPU 41x?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
Numero di ordinazione:

Contents
The procedure is given in the attached PDF document with the following contents.

1 Introduction
2 Preliminary Considerations
   2.1 When should you use an HMI station and when a PC station?
   2.2 Which PROFIBUS CP should you select?
3 Connecting a Panel via PROFIBUS
   3.1 Requirements
   3.2 ‪‪Configuration in STEP 7 and WinCC flexible as well as on the panel
4 Connecting WinCC flexible Runtime to SIMATIC S7-300/400 Without
   Station Configuration Editor
   4.1 Requirements
   4.2 Connecting an HMI station
   4.3 Connecting a PC station
5 Connecting a WinCC flexible Runtime to SIMATIC S7-300/400 With
   Station Configuration Editor
   5.1 Requirements
   5.2 Connecting an HMI station
   5.3 Connecting a PC station

WinCC_flexible_Kommunikation_Profibus_V10_e.pdf ( 1168 KB )

Keywords
300 series, 400 series, Connection, Connect, Operator panel, Display, Communication, Drivers, Controller, PLC, MPI/DP interface, IF1B MPI/DP, Baud rate, Address, Only master on the bus, Controller connection

 Articolo con ID:42918861   Data:2010-06-07 
Questo articoloè stato utilenon è stato utile                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
Vai all'articolo
Stampa
Creazione PDF 
Invia l'articolo
QuickLinks
Strumento di compatibilità 
Aiuto
Aiuto on-line
Guided Tour