Contents The procedure is given in the attached PDF document with the following contents.
1 Introduction
2 Preliminary Considerations
2.1 When should you use an HMI station and when a PC station?
2.2 Which PROFIBUS CP should you select?
3 Connecting a Panel via PROFIBUS
3.1 Requirements
3.2 Configuration in STEP 7 and WinCC flexible as well as on the panel
4 Connecting WinCC flexible Runtime to SIMATIC S7-300/400 Without
Station Configuration Editor
4.1 Requirements
4.2 Connecting an HMI station
4.3 Connecting a PC station
5 Connecting a WinCC flexible Runtime to SIMATIC S7-300/400 With
Station Configuration Editor
5.1 Requirements
5.2 Connecting an HMI station
5.3 Connecting a PC station
WinCC_flexible_Kommunikation_Profibus_V10_e.pdf ( 1168 KB )
Keywords 300 series, 400 series, Connection, Connect, Operator panel, Display, Communication, Drivers, Controller, PLC, MPI/DP interface, IF1B MPI/DP, Baud rate, Address, Only master on the bus, Controller connection
|