show the entry list
WinCC flexible ES -- Working with projects -- Upgrading to new version
How do you migrate a WinCC flexible 2008 SP3 project to WinCC V11 (TIA Portal) V11 SP2 in Windows 7 64-bit?
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
How do you migrate a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)?
How can you transfer global libraries from WinCC flexible to WinCC (TIA Portal)?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
What are the solutions offered for working with different versions of WinCC flexible?
How do you migrate a ProTool project with SIMOTION CPU connection to a WinCC flexible project and SIMOTION SCOUT?
What connections are there between the version designations in WinCC flexible?
How do you adapt tag names to the name structure of WinCC flexible after a ProTool migration?
Which changes have to be made in WinCC flexible 2004 SP1 when changing over from TP 170micro to TP 177micro or from TP 170A to TP 177A?
WinCC flexible ES -- Working with projects -- Creating, editing, archiving and copying projects
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How can you change the column width of picture objects in WinCC flexible?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
What are the solutions offered for working with different versions of WinCC flexible?
Which problems might arise if the "log.LDF" file is not available in a WinCC flexible project?
Why does WinCC flexible close again automatically after the program start?
How can you save WinCC flexible projects / libraries as projects / libraries in the format of an earlier version of WinCC flexible?
How can you delete unused tags or objects from a WinCC flexible project?
What options do you have for copying pictures from one WinCC flexible project to another?
Copying HMI projects integrated in SIMATIC STEP 7 at file level
How can you open a WinCC project integrated in STEP 7 faster?
How do you archive projects in WinCC flexible and which files are required?
How do you back transfer the projects of an operator panel and what should you watch out for?
What transfer options are available in the various operator panels?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
Part number:

Description
As from WinCC flexible 2008 SP2 it is possible to operate WinCC flexible Runtime in widescreen mode. If you want to convert your 4:3 project into a widescreen project, it is recommended to disable the setting "Fit screen and screen objects to new HMI device".
This setting is enabled by default in WinCC flexible and means that when you change to widescreen mode, all the picture objects are stretched and lose their original shape.

Instructions
Proceed as described in the table below to disable the setting "Fit screen and screen objects to new HMI device".
 
No. Procedure
1 Open your WinCC flexible project.
2 Open the Settings dialog and via "Screen editor > Screen options > Settings" you disable the option "Fit screen and screen objects to new HMI device".


Fig. 01

3 Now you can change the screen resolution in the device settings.

More information on the topic of "Operator panel dependency of projects" is available in the manual.

Keywords
Distortion, Distorted pictures, Distorted picture, Truncated pictures, Truncated picture, Aspect ratio, Picture format, Widescreen

 Entry ID:42713776   Date:2010-05-12 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour