show the entry list
PCDiagBridge
Part number:

Description
Attached is the new "PCDiagBridge V1.04.7" diagnostics software that you can download free of charge.

"PCDiagBridge" is a software tool that reads out the diagnostics data from SIMATIC IPCs, SITOP USVs, WinAC RTX and WinAC RTX F and makes it available to the SIMATIC HMI software products WinCC and WinCC flexible. You can use "PCDiagBridge" to monitor the following hardware and software components:

  • SIMATIC IPC hardware (fan speed, CPU temperature, CMOS voltage and mass storage, for example)
  • SITOP UPS (operating mode, error message, switch-off)
  • Operating and monitoring of the WinAC RTX / WinAC RTX F (Run/Stop, error display, operating mode)

The "PCDiagBridge" user interface provides you with all the relevant PC diagnostics data at a glance. Prepared templates for WinCC and WinCC flexible permit easy integration of the diagnostics data into the SIMATIC visualization system.

Note
If you require one of the following functions:

  • Monitoring of networked SIMATIC IPCs
  • Reading out and sending of error messages via OPC server, e-mail or SMS
  • Worldwide monitoring of SIMATIC IPCs via Web browser

we recommend using "SIMATIC IPC DiagMonitor". More information about the "SIMATIC IPC DiagMonitor" is available in Entry ID: 43192661 and at:
www.siemens.com/simatic-pc

Hardware requirements
This entry was created for "PCDiagBridge V1.04.7" and can run on the SIMATIC IPCs below:

  • SIMATIC Microbox PC 427B
  • SIMATIC IPC427C
  • SIMATIC IPC627C
  • SIMATIC IPC227D
  • SIMATIC IPC277D
  • SIMATIC Box PC 627B
  • SIMATIC Box PC 827B
  • SIMATIC HMI IPC477C
  • SIMATIC HMI IPC477C PRO
  • SIMATIC HMI IPC577C
  • SIMATIC HMI IPC677C
  • Panel PC 477B
  • Panel PC 577B
  • Panel PC 677B
  • SIMATIC Rack PC 547B
  • Rack PC 647B
  • Rack PC 847B
  • SIMATIC Rack PC IL 43
  • SIMATIC IPC547C
  • SIMATIC IPC647C
  • SIMATIC IPC847C
  • SIMATIC IPC547D
  • All versions of WinAC RTX / WinAC RTX F
  • All SITOP UPSs with USB interface

Software requirements
"PCDiagBridge V1.04.7" runs on the operating systems below:

  • Windows 2000 Professional
  • Windows XP Professional
  • Windows XP Embedded (SIMATIC IPC configuration)
  • Windows XP Embedded Standard 2009 (SIMATIC IPC configuration)
  • Windows Server 2003 Edition (32-bit)
  • Windows Server 2008 Edition (32-bit)
  • Windows Vista Ultimate (32-bit)
  • Microsoft Windows 7 (32-bit)
The following software must be installed in order to use "PCDiagBridge V1.04.7":
  • Microsoft Visual Basic 6.0 runtime files
  • Microsoft WinSock Control 6.0 MSWINSCK.OCX
  • Microsoft Rich Textbox Control 6.0 RICHTX32.OCX
  • SIMATIC IPC DiagBase as from version V1.1
    Remark: The SIMATIC IPC DiagBase user interfaces "Management Explorer" and "Alarm Manager" can be operated in parallel, but are not requirements for PCDiagBridge. You can disable the automatic start of the Management Explorer and the Alarm Manager when Windows starts. 
  • SITOP UPS USB driver FTD2XX.SYS (only if SITOP UPS is available)

Using the "PCDiagBridge V1.04.7" diagnostics software allows you to recognize any possible disturbances with SIMATIC IPCs at an early stage. SIMATIC IPC error messages to the operating personnel help to avoid or reduce system downtimes.

Download
 

PCDiagBridge

Version Download Remarks
Version 1.04.7 PCDiagBridgeSetup_V1_04_7.zip ( 634 KB ) Current version
Version 1.04.0003 PCDiagBridgeSetup_V1_4_0003.zip ( 637 KB )  
Version 1.04.0001

PCDiagBridgeSetup_V1_4_0001.zip ( 636 KB )

 
Version 1.03.0001

PCDiagBridgeSetup_V1_3_0001.zip ( 635 KB )

 
Version 1.01.0001

PCDiagBridgeSetup_V1_1_0001.zip ( 720 KB )

 

More information and sample applications
The "SIMATIC IPC DiagBase" software is available for downloading free of charge in
Entry ID: 29316343 .

An example of how to incorporate "SIMATIC IPC DiagBase" and "PCDiagBridge" in your WinCC or WinCC flexible projects is available in
Entry IDs: 29855065 (WinCC) and 31492549 (WinCC flexible).

 Entry ID:42674746   Date:2012-03-26 
I regard this article....as helpfulas not helpful                                 
related links
SIMATIC IPC DiagBase Download
SIMATIC IPC BIOS Manager
SIMATIC IPC DiagMonitor
DiagMonitor Installation of the ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour