|
Description Software Redundancy (SWR) is a software package for configuring fault-tolerant controllers with standard components. The controller part consists of standard CPUs of the S7-300 and S7-400 series. The redundancy link for synchronizing the redundant CPUs is achieved with standard communication mechanisms like CPs or via an MPI interface. Connection to I/O devices is via two redundant PROFIBUS DP segments to the ET-200M stations with redundant IM 153-2 interface modules. You can also implement Software Redundancy on WinAC RTX as from version 2008.
Note
More information is available in the function manual "Software Redundancy for SIMATIC S7" in Entry ID 1137637.
The following table lists modules that support software redundancy. The lowercase letter x is a wildcard character in the order numbers.
S7-300 CPUs
| Module |
Order number |
| CPU 313C-2 DP |
6ES7313-6CE0x-0AB0
6ES7313-6CF03-0AB0
6ES7313-6CG04-0AB0 |
| CPU 314C-2 DP |
6ES7314-6CF0x-0AB0
6ES7314-6CG0x-0AB0
6ES7314-6EH04-0AB0 |
| CPU 315-2 DP |
6ES7315-2AFxx-0AB0
6ES7315-2AG10-0AB0
6ES7315-2AH14-0AB0 |
| CPU 315F-2 DP |
6ES7315-6FF0x-0AB0 |
| CPU 315-2 PN/DP |
6ES7315-2EG10-0AB0
6ES7315-2EH1x-0AB0 |
| CPU 315F-2 PN/DP |
6ES7315-2FH1x-0AB0
6ES7315-2FJ14-0AB0 |
| CPU 315T-2 DP |
6ES7315-6Tx1x-0AB0 |
| CPU 316-2 DP |
6ES7316-2AG0x-0AB0 |
| CPU 317-2 DP |
6ES7317-2AJ10-0AB0
6ES7317-2AK14-0AB0 |
| CPU 317F-2 DP |
6ES7317-6FF0x-0AB0 |
| CPU 317-2 PN/DP |
6ES7317-2Ex1x-0AB0 |
| CPU 317F-2 PN/DP |
6ES7317-2Fx1x-0AB0 |
| CPU 317T-2 DP |
6ES7317-6Tx1x-0AB0 |
| CPU 318-2 DP |
6ES7318-2AJ0x-0AB0 |
| CPU 319-3 PN/DP |
6ES7318-3EL0x-0AB0 |
| CPU 319F-3 PN/DP |
6ES7318-3FL0x-0AB0 |
Table 01
S7-400 CPUs
| Module |
Order number |
| CPU 412-1 |
6ES7412-1XF0x-0AB0
6ES7412-1XJ05-0AB0 |
| CPU 412-2 PN |
6ES7412-2EK06-0AB0 |
| CPU 412-2 |
6ES7412-2XG0x-0AB0
6ES7412-2XJ05-0AB0 |
| CPU 413-1 |
6ES7413-1XG0x-0AB0 |
| CPU 413-2 |
6ES7413-2XG0x-0AB0 |
| CPU 414-1 |
6ES7414-1XG0x-0AB0 |
| CPU 414-2 |
6ES7414-2XG0x-0AB0
6ES7414-2XJ0x-0AB0
6ES7414-2XK05-0AB0 |
| CPU 414-3 |
6ES7414-3XJ0x-0AB0
6ES7414-3XM05-0AB0 |
| CPU 414-3 PN/DP |
6ES7414-3EM05-0AB0
6ES7414-3EM06-0AB0 |
| CPU 414F-3 PN/DP |
6ES7414-3FM06-0AB0 |
| CPU 416-1 |
6ES7416-1XJ0x-0AB0 |
| CPU 416-2 |
6ES7416-2XK0x-0AB0
6ES7416-2XL0x-0AB0
6ES7416-2XN05-0AB0 |
| CPU 416F-2 |
6ES7416-2FN05-0AB0 |
| CPU 416-3 |
6ES7416-3XL0x-0AB0
6ES7416-3XR05-0AB0 |
| CPU 416-3 PN/DP |
6ES7416-3ES06-0AB0
6ES7416-3ER05-0AB0 |
| CPU 416F-3 PN/DP |
6ES7416-3FR05-0AB0
6ES7416-3FR06-0AB0 |
| CPU 417-4 |
6ES7417-4XL0x-0AB0
6ES7417-4XT05-0AB0 |
Table 02
Note The SIMATIC S7-300/400 F-CPUs are to be used here without F program.
Communication modules with DP master function
| Module |
Order number |
CP 443-5 EXT
(connection to PROFIBUS network) |
6GK7443-5DX04-0XE0
6GK7443-5DX05-0XE0 |
IM 467 and IM 467-FO
(can only be used in version V1.1) |
6ES7467-5GJ0x-0AB0
6ES7467-5FJ00-0AB0 |
Table 03
Communication modules for linking the stations
| Module |
Order number |
| CP 342-5 |
6GK7342-5DA00-0XE0
6GK7342-5DA02-0XE0
6GK7342-5DA03-0XE0 |
| CP 343-1 |
6GK7343-1BA00-0XE0
6GK7343-1EX11-0XE0
6GK7343-1EX30-0XE0
6GK7343-1GX30-0XE0 |
CP 343-1 LEAN
(connection to Industrial Ethernet) |
6GK7343-1CX10-0XE0 |
CP 443-5 EXT
(connection to PROFIBUS network) |
6GK7443-5DX04-0XE0
6GK7443-5DX05-0XE0 |
CP 443-1 ISO1
(connection to Industrial Ethernet) |
6GK7443-1EXxx-0XE0
6GK7443-1GXxx-0XE0
6GK7443-1BXxx-0XE0 |
Table 04
Modules for distributed I/O device ET 200M
| Module |
Order number |
| IM 153-2 |
6ES7153-2BA0x-0XB0 as from release 2
(bus module 6ES7195-7HD10-0XA0) |
| FM 350-1 |
6ES7350-1AH0x-0AE0 |
CP 341
(20 mA TTY, RS232, RS422/485) |
6ES7341-1xH01-0AE0
6ES7341-1xH02-0AE0 |
CP 341
(RS232C) |
6ES7341-1AH02-0AE0 |
| All digital and analog modules for ET 200M (see Catalog ST70) |
Table 05
PC-based controller
| Module |
Order number |
| Windows Logic Controller WinAC RTX F V4 |
6ES7611-4FB00-0YB7
You cannot order this MLFB separately but only as part of the products below.
- WinAC RTX F as from version 2009 (6ES7 671-1RC0x-0YA0)
- SIMATIC IPC427 Bundles (6ES7 675-1D...)
- SIMATIC HMI IPC477C Bundles(6AV7 884-...)
|
| Windows Logic Controller WinAC RTX V4 |
6ES7611-4SB00-0YB7
You cannot order this MLFB separately but only as part of the products below.
- WinAC RTX as from version 4 (6ES7 671-0RC0x-0YA0)
- Microbox 420-RTX (6ES7 675-1B...)
- Microbox 427B Bundles (6ES7 675-1C...)
- IPC427C Bundles (6ES7 675-1D...)
- Panel PC 477 HMI/RTX (6AV7 84...)
- Panel PC 477B Bundles (6AV7 85...)
- HMI IPC477C Bundles (6AV7 884...)
|
| Embedded Controller, EC31 |
6ES7677-1DD00-0BA0
6ES7677-1DD10-0BA0 |
| Embedded Controller, EC31-RTX |
6ES7677-1DD00-0BB0
6ES7677-1DD10-0BB0 |
| Embedded Controller, EC31 HMI/RTX |
6ES7677-1DD00-0BF0
6ES7677-1DD00-0BG0
6ES7677-1DD00-0BH0
6ES7677-1DD10-0BF0
6ES7677-1DD10-0BG0
6ES7677-1DD10-0BH0 |
| Embedded Controller, EC31-RTX F |
6ES7677-1FD00-0FB0
6ES7677-1FD10-0FB0 |
Table 06
Note
The ET 200M stations must always be configured with active bus modules (6ES7195-7HB00-0XA0 or 6ES7195-7HC00-0XA0), even if the "Hot swapping of I/O modules" function is not possible with S7-300 CPUs.
|