show the entry list
S7-300 CPU 31x -- Product information -- Technical data
How many modules can you slot on an S7-300 mounting rail?
How can you control the ALM (Active Line Module) of a CU320 (with DriveCLIQ) with the SIMATIC program?
Where can you find an update to use the SINAMICS with newer firmware in S7 Technology V4.1?
Which modules can you use when implementing software redundancy?
Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails?
How do you find out further technical information about your module?
Why can't I see the values which are transmitted to an unlinked destination DB with SFC84, even though SFC84 is not indicating an error (RET_VAL = W#16#000?
How does the CPU 31x/31xC/C7 react when an MMC fault occurs during the save procedure?
What is the effect of the STEP 7 function "Copy RAM to ROM"?
Why does the SFC 54 "RD_DPARM" not work with the new S7-300 CPU with MMC?
How do you copy the user program from the load memory into the main memory without PG with a S7-300 CPU with MC slot?
How can you backup your program from the load memory?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
At which ambient temperature and at which air pressure can you operate a SIMATIC S7-300?
What can you do when the power requirement of the modules in the subrack exceeds the power supply provided by the CPU on the backplane bus?
Where do you find certificates and approvals for SIMATIC S7 in the Internet?
Where can you find images, graphics, symbols and screenshots for SIMATIC industrial automation systems?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
S7-400 CPU 41x -- Product information -- Technical data
Why is the download procedure with an S7-400 CPU aborted with the error message "D223"?
What are the functional restrictions of old releases and firmware versions for the S7-400 CPUs operating in conjunction with the CP443-5 Extended V6.1?
Which modules can you use when implementing software redundancy?
Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails?
How do you find out further technical information about your module?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
Where can you find images, graphics, symbols and screenshots for SIMATIC industrial automation systems?
Where do you find certificates and approvals for SIMATIC S7 in the Internet?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
Retentivity behavior of S7-400 CPUs and the CPU 318-2 CPUs
S7-400: Operating Mode Switch at the new CPU 41x (as of FW Version 4.0)
Industrial Ethernet S7-300/400 CPs -- Product information -- System description (protocols)
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What should you watch out for when you enable the "SNMP" function in the configuration of the security module?
Which security modules support dynamic DNS and can use it to communicate with each other?
What should you watch out for when enabling and using the security functions of CP343-1 Advanced and CP443-1 Advanced?
What should you watch out for when upgrading from previous modules to the successor module CP443-1 or CP443-1 Advanced?
How do you verify the authenticity of the Siemens modules CP343-1 and CP443-1?
What should you watch out for when operating a port of CP343-1, 6GK7343-1CX10-0XE0 and 6GK7343-1EX30-0XE0 with firmware V2.1 or higher, with 10 Mbit/s half duplex?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Where do you procure the firmware extension for the CP 343-1 ERPC for database connection?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which modules can you use when implementing software redundancy?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Using C-PLUG with network components and SIMATIC CPs
What properties have the communication services and protocols that can be used in the Industrial Ethernet network?
Behavior of the communication processors during data transfer via TCP connections without RFC 1006
What should you watch out for with the ICMP Redirect (Internet control message protocol) function regarding the IP address of the router used for Industrial Ethernet CPs?
What should you pay attention to with the autonegotiation function for negotiating the LAN mode in Industrial Ethernet CPs?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which modules support the S7 routing function?
In the case of open TCP/IP communication via Industrial Ethernet using T blocks with IE CPs and CPUs, why are different amounts of messages sent when the maximum length of 1452 bytes of user data is transferred?
What properties, advantages and special features does the ISO protocol offer?
What properties, advantages and special features does the UDP protocol offer?
What properties, advantages and special features does the ISO-on-TCP protocol offer?
What properties, advantages and special features does the S7 protocol offer?
What properties, advantages and special features does the TCP protocol offer?
What are the requirements for disabling the PROFINET CBA interface for CP443-1EX40?
"Time Wait" with TCP connection setup
What are the different data block lengths for the various protocols of Send/Receive communication?
What is RFC1006 and what do I need this service for?
Meaning and function of the "Keep Alive" in TCP connections
ET 200M (standard modules) -- Product information -- Technical data
Which modules can you use when implementing software redundancy?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
Multiline set-up of ET200M
How many modules can you operate with one interface module of the ET 200M?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
How do you assign and identify thermocouples?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
PROFIBUS S7-300/400 CPs -- Product information -- System description
What is the difference between "normal routing" and data record routing?
Which modules can you use when implementing software redundancy?
What are the functional restrictions of old releases and firmware versions for the S7-400 CPUs operating in conjunction with the CP443-5 Extended V6.1?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Meaning of the numeric display in the NCM diagnostics buffer
Which protocols does CP 342-5 support?
Different block behavior of the FC5 and FC50 for Ind. Ethernet S7 300 CPs
Which modules support the S7 routing function?
What properties, advantages and special features does the DP protocol offer?
What properties, advantages and special features does the FMS protocol offer?
What properties, advantages and special features does the S7 protocol offer?
What properties, advantages and special features does the FDL protocol offer?
Serial CPs -- Product information -- Technical data
Which modules can you use when implementing software redundancy?
What protocols for the point-to-point connection are supported by CPs in S7-300 / S7-400 and where can you get further information?
CP340-Functions
How do you define the levels of CP 340 / CP 341 / CP 440 / CP 441 with RS 485/X.27?
CP441 functions
CP341-Functions
Possible baud rates for S7-400 PtP communication
Maximum number of centrally slottable CP 340s
Possible transfer rates of the CP 341 depending on the interface
S7-400 IM Modules -- Product information -- Technical data
Which modules can you use when implementing software redundancy?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Cables for S7-400 interface modules (IM 46x) in standard lengths and special lengths
Supplements on Hardware Configuration of CiR
S7-300 IM Modules -- Setting up and parameterizing hardware -- Connecting and wiring modules
Which modules can you use when implementing software redundancy?
How do you operate an IM174 on the clock-synchronized PROFIBUS of an FM458-1DP?
Using an FM350 in an extended configuration (with IM365)
Which connecting cables are there for IM 360/361?
IM 365: SM and FM modules that can be used in Rack 1
FM 350-1, 350-2, 450, SM338 -- Product information -- Determining performance and quantity frameworks
Which modules can you use when implementing software redundancy?
FM350-1: changing the updating time in measuring modes
WinAC RTX -- Product information -- System description
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Which modules can you use when implementing software redundancy?
Which modules support the S7 routing function?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Which modules can you use when implementing software redundancy?
Part number:

Description
Software Redundancy (SWR) is a software package for configuring fault-tolerant controllers with standard components. The controller part consists of standard CPUs of the S7-300 and S7-400 series. The redundancy link for synchronizing the redundant CPUs is achieved with standard communication mechanisms like CPs or via an MPI interface. Connection to I/O devices is via two redundant PROFIBUS DP segments to the ET-200M stations with redundant IM 153-2 interface modules. You can also implement Software Redundancy on WinAC RTX as from version 2008.

Note
More information is available in the function manual "Software Redundancy for SIMATIC S7" in Entry ID 1137637.

The following table lists modules that support software redundancy. The lowercase letter x is a wildcard character in the order numbers.

S7-300 CPUs
 
Module Order number
CPU 313C 6ES7313-5BF03-0AB0
6ES7313-5BG04-0AB0
CPU 313C-2 PTP 6ES7313-6BF03-0AB0
6ES7313-6BG04-0AB0
CPU 313C-2 DP 6ES7313-6CE0x-0AB0
6ES7313-6CF03-0AB0
6ES7313-6CG04-0AB0
CPU 314 6ES7314-1AG1x-0AB0
CPU 314C-2PTP 6ES7314-6BG03-0AB0
6ES7314-6BH04-0AB0
CPU 314C-2 DP 6ES7314-6CF0x-0AB0
6ES7314-6CG0x-0AB0
6ES7314-6EH04-0AB0
CPU 315-2 DP 6ES7315-2AFxx-0AB0
6ES7315-2AG10-0AB0
6ES7315-2AH14-0AB0
CPU 315F-2 DP 6ES7315-6FF0x-0AB0
CPU 315-2 PN/DP 6ES7315-2EG10-0AB0
6ES7315-2EH1x-0AB0
CPU 315F-2 PN/DP 6ES7315-2FH1x-0AB0
6ES7315-2FJ14-0AB0
CPU 315T-2 DP 6ES7315-6Tx1x-0AB0
CPU 316-2 DP 6ES7316-2AG0x-0AB0
CPU 317-2 DP 6ES7317-2AJ10-0AB0
6ES7317-2AK14-0AB0
CPU 317F-2 DP 6ES7317-6FF0x-0AB0
CPU 317-2 PN/DP 6ES7317-2Ex1x-0AB0
CPU 317F-2 PN/DP 6ES7317-2Fx1x-0AB0
CPU 317T-2 DP 6ES7317-6Tx1x-0AB0
CPU 318-2 DP 6ES7318-2AJ0x-0AB0
CPU 319-3 PN/DP 6ES7318-3EL0x-0AB0
CPU 319F-3 PN/DP 6ES7318-3FL0x-0AB0
Table 01

S7-400 CPUs
 
Module Order number
CPU 412-1 6ES7412-1XF0x-0AB0
6ES7412-1XJ05-0AB0
CPU 412-2 PN 6ES7412-2EK06-0AB0
CPU 412-2 6ES7412-2XG0x-0AB0
6ES7412-2XJ05-0AB0
CPU 413-1 6ES7413-1XG0x-0AB0
CPU 413-2 6ES7413-2XG0x-0AB0
CPU 414-1 6ES7414-1XG0x-0AB0
CPU 414-2 6ES7414-2XG0x-0AB0
6ES7414-2XJ0x-0AB0
6ES7414-2XK05-0AB0
CPU 414-3 6ES7414-3XJ0x-0AB0
6ES7414-3XM05-0AB0
CPU 414-3 PN/DP 6ES7414-3EM05-0AB0
6ES7414-3EM06-0AB0
CPU 414F-3 PN/DP 6ES7414-3FM06-0AB0
CPU 416-1 6ES7416-1XJ0x-0AB0
CPU 416-2 6ES7416-2XK0x-0AB0
6ES7416-2XL0x-0AB0
6ES7416-2XN05-0AB0
CPU 416F-2 6ES7416-2FN05-0AB0
CPU 416-3 6ES7416-3XL0x-0AB0
6ES7416-3XR05-0AB0
CPU 416-3 PN/DP 6ES7416-3ES06-0AB0
6ES7416-3ER05-0AB0
CPU 416F-3 PN/DP 6ES7416-3FR05-0AB0
6ES7416-3FR06-0AB0
CPU 417-4 6ES7417-4XL0x-0AB0
6ES7417-4XT05-0AB0
Table 02

Note
The SIMATIC S7-300/400 F-CPUs are to be used here without F program.

Communication modules with DP master function
 
Module Order number
CP 443-5 EXT
(connection to PROFIBUS network)
6GK7443-5DX04-0XE0
6GK7443-5DX05-0XE0
IM 467 and IM 467-FO
(can only be used in version V1.1)
6ES7467-5GJ0x-0AB0
6ES7467-5FJ00-0AB0
Table 03

Communication modules for linking the stations
 
Module Order number
CP 342-5 6GK7342-5DA00-0XE0
6GK7342-5DA02-0XE0
6GK7342-5DA03-0XE0
CP 343-1 6GK7343-1BA00-0XE0
6GK7343-1EX11-0XE0
6GK7343-1EX30-0XE0
6GK7343-1GX30-0XE0
CP 343-1 LEAN
(connection to Industrial Ethernet)
6GK7343-1CX10-0XE0
CP 443-5 EXT
(connection to PROFIBUS network)
6GK7443-5DX04-0XE0
6GK7443-5DX05-0XE0
CP 443-1 ISO1
(connection to Industrial Ethernet)
6GK7443-1EXxx-0XE0
6GK7443-1GXxx-0XE0
6GK7443-1BXxx-0XE0
Table 04

Modules for distributed I/O device ET 200M
 
Module Order number
IM 153-2 6ES7153-2BA0x-0XB0 as from release 2
(bus module 6ES7195-7HD10-0XA0)
FM 350-1 6ES7350-1AH0x-0AE0
CP 341
(20 mA TTY, RS232, RS422/485)
6ES7341-1xH01-0AE0
6ES7341-1xH02-0AE0
CP 341
(RS232C)
6ES7341-1AH02-0AE0
All digital and analog modules for ET 200M (see Catalog ST70)
Table 05

PC-based controller
 
Module Order number
Windows Logic Controller WinAC RTX F V4 6ES7611-4FB00-0YB7
You cannot order this MLFB separately but only as part of the products below.
  • WinAC RTX F as from version 2009 (6ES7 671-1RC0x-0YA0)
  • SIMATIC IPC427 Bundles (6ES7 675-1D...)
  • SIMATIC HMI IPC477C Bundles(6AV7 884-...)
Windows Logic Controller WinAC RTX V4 6ES7611-4SB00-0YB7
You cannot order this MLFB separately but only as part of the products below.
  • WinAC RTX as from version 4 (6ES7 671-0RC0x-0YA0)
  • Microbox 420-RTX (6ES7 675-1B...)
  • Microbox 427B Bundles (6ES7 675-1C...)
  • IPC427C Bundles (6ES7 675-1D...)
  • Panel PC 477 HMI/RTX (6AV7 84...)
  • Panel PC 477B Bundles (6AV7 85...)
  • HMI IPC477C Bundles (6AV7 884...)
Embedded Controller, EC31 6ES7677-1DD00-0BA0
6ES7677-1DD10-0BA0
Embedded Controller, EC31-RTX 6ES7677-1DD00-0BB0
6ES7677-1DD10-0BB0
Embedded Controller, EC31 HMI/RTX 6ES7677-1DD00-0BF0
6ES7677-1DD00-0BG0
6ES7677-1DD00-0BH0
6ES7677-1DD10-0BF0
6ES7677-1DD10-0BG0
6ES7677-1DD10-0BH0
Embedded Controller, EC31-RTX F 6ES7677-1FD00-0FB0
6ES7677-1FD10-0FB0
Table 06  

Note
The ET 200M stations must always be configured with active bus modules (6ES7195-7HB00-0XA0 or 6ES7195-7HC00-0XA0), even if the "Hot swapping of I/O modules" function is not possible with S7-300 CPUs.

 Entry ID:42614519   Date:2013-08-07