Description One connection resource is required in the S7-400 CPU for each of the following communication connections of the Industrial Ethernet CP:
| Communication connection |
Service |
TSAP |
| PG communication via S7 server |
- Web diagnostics, e.g. for displaying the diagnostics buffer of the CPU
- Set time in CPU 318
- Applets, e.g. to read MLFB or status of the CPU
|
0x01 |
| System connection via S7 server |
- FTP server (read and write access to file DBs)
- FTP client (read and write access to file DBs)
- Applets (read and write access to CPU data)
|
0x03 |
| System connection |
|
0x0F |
If the SEND / RECEIVE, FTP and Web diagnostics services are used simultaneously in the Industrial Ethernet, 3 connection resources of the S7-400 CPU are occupied.
An Industrial Ethernet CP occupies a maximum of 3 connection resources in the S7-400 CPU, i.e. maximum one connection resource for:
- PG communication via S7 server (TSAP=0x01)
- System connection via S7 server (TSAP=0x03)
- System connection SEND/RECEIVE (TSAP=0x0F)
|