show the entry list
Industrial Ethernet S7-300/400 CPs -- Product information -- Determining performance and quantity frameworks
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Which connection resources are occupied in the S7-300 CPU for communication connections and services of the Industrial Ethernet CP?
Which connection resources are occupied in the S7-400 CPU for communication connections and services of the Industrial Ethernet CP?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
Increasing the CPU load for a data length of greater than 240 bytes in the case of Send/Receive communication with Industrial Ethernet CPs
What RAM capacity does the CP 343-1 IT make available for FTP services?
Why under certain circumstances are there very long response times with TCP connections?
S7-400 CPU 41x -- Product information -- Determining performance and quantity frameworks
How can you change the size of the available free main memory of a SIMATIC S7-400 CPU?
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Which connection resources are occupied in the S7-400 CPU for communication connections and services of the Industrial Ethernet CP?
How many breakpoints can you insert when debugging a program?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
How can you determine the size of the load memory and main memory of a SIMATIC S7-300/400 CPU?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
What is a hardware interrupt and how do they work in the S7-400 system?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
Which connection resources are occupied in the S7-400 CPU for communication connections and services of the Industrial Ethernet CP?
Part number:

Description
One connection resource is required in the S7-400 CPU for each of the following communication connections of the Industrial Ethernet CP:
 
Communication connection Service TSAP
PG communication via S7 server
  • Web diagnostics, e.g. for displaying the diagnostics buffer of the CPU
  • Set time in CPU 318
  • Applets, e.g. to read MLFB or status of the CPU
0x01
System connection via S7 server
  • FTP server (read and write access to file DBs)
  • FTP client (read and write access to file DBs)
  • Applets (read and write access to CPU data)
0x03
System connection
  • SEND and RECEIVE
0x0F

If the SEND / RECEIVE, FTP and Web diagnostics services are used simultaneously in the Industrial Ethernet, 3 connection resources of the S7-400 CPU are occupied.

An Industrial Ethernet CP occupies a maximum of 3 connection resources in the S7-400 CPU, i.e. maximum one connection resource for:

  • PG communication via S7 server (TSAP=0x01)
  • System connection via S7 server (TSAP=0x03)
  • System connection SEND/RECEIVE (TSAP=0x0F)

 Entry ID:42480718   Date:2010-04-26 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour