show the entry list
Industrial Ethernet S7-300/400 CPs -- Product information -- Determining performance and quantity frameworks
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Which connection resources are occupied in the S7-300 CPU for communication connections and services of the Industrial Ethernet CP?
Which connection resources are occupied in the S7-400 CPU for communication connections and services of the Industrial Ethernet CP?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
Increasing the CPU load for a data length of greater than 240 bytes in the case of Send/Receive communication with Industrial Ethernet CPs
What RAM capacity does the CP 343-1 IT make available for FTP services?
Why under certain circumstances are there very long response times with TCP connections?
S7-300 CPU 31x -- Product information -- Determining performance and quantity frameworks
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Which connection resources are occupied in the S7-300 CPU for communication connections and services of the Industrial Ethernet CP?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
How can you determine the size of the load memory and main memory of a SIMATIC S7-300/400 CPU?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
What is a hardware interrupt and how do they work in the S7-300 system?
What is the maximum number of OPs that a CPU S7-300 can communicate with?
What can you do when the power requirement of the modules in the subrack exceeds the power supply provided by the CPU on the backplane bus?
Does PROFIBUS DP communication use connection resources?
What is the maximum number of CP modules that can be slotted in a SIMATIC S7-300/400 station?
Why, in the case of a networked SIMATIC S7, does the connection to the OP clear down when you call diagnostics functions with the PG or transfer blocks?
How many breakpoints can you insert when debugging a program?
Which connection resources are occupied in the S7-300 CPU for communication connections and services of the Industrial Ethernet CP?
Part number:

Description
One connection resource is required in the S7-300 CPU for each of the following communication connections of the Industrial Ethernet CP.
 
Communication connection Service TSAP
PG communication via S7 server
  • Web diagnostics, for example for displaying the diagnostics buffer of the CPU
  • Set time in CPU 318
  • Applets, for example to read MLFB or status of the CPU
  • Bacnet (read system status list (SSL))
  • ERPC (read system status list (SSL))
0x01
System connection via S7 server
  • FTP server (read and write access to file DBs)
  • FTP client (read and write access to file DBs)
  • Applets (read and write access to CPU data)
  • Bacnet (read and write access to CPU data)
  • ERPC (read and write access to CPU data)
0x03
System connection
  • FETCH and WRITE via SEND/RECEIVE connection
  • PBC for OP multiplexer
0x03

If the FETCH / WRITE, PBC for multiplexer, FTP and Web diagnostics services are used simultaneously in the Industrial Ethernet, 4 connection resources of the S7-300 CPU are occupied.
An Industrial Ethernet CP can occupy, for example, a maximum of 4 connection resources in the S7-300 CPU; this one connection resource each for:

  • PG communication via S7 server (TSAP=0x01)
  • System connection via S7 server (TSAP=0x03)
  • System connection SEND/RECEIVE (TSAP=0x03)
  • System connection OP multiplexer (TSAP=0x03)
Note
In the manual for the S7-300 CPUs under "Technical Details" you will find information about the maximum number of communications processors (CPs) that can be operated.
The manual of the S7-300 CPUs is available for downloading in Entry ID: 12996906.

 Entry ID:42480411   Date:2011-04-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour